Data Fields
CAN_Config_ Struct Reference

CAN Global configuration. More...

#include <CAN.h>

Collaboration diagram for CAN_Config_:
Collaboration graph
[legend]

Data Fields

CAN_Objectobject
 
const CAN_HWAttrshwAttrs
 

Detailed Description

CAN Global configuration.

The CAN_Config structure contains a set of pointers used to characterize the CAN driver implementation.

Field Documentation

§ object

CAN_Object* CAN_Config_::object

Pointer to a driver specific data object

§ hwAttrs

const CAN_HWAttrs* CAN_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale