Data Fields
MCAN_TxEventFifoStatus Struct Reference

Structure for MCAN Tx Event FIFO Status. More...

#include <MCAN.h>

Data Fields

uint32_t fillLvl
 
uint32_t getIdx
 
uint32_t putIdx
 
uint32_t fifoFull
 
uint32_t eleLost
 

Detailed Description

Structure for MCAN Tx Event FIFO Status.

Field Documentation

§ fillLvl

uint32_t MCAN_TxEventFifoStatus::fillLvl

Event FIFO Fill Level

§ getIdx

uint32_t MCAN_TxEventFifoStatus::getIdx

Event FIFO Gut Index

§ putIdx

uint32_t MCAN_TxEventFifoStatus::putIdx

Event FIFO Put Index

§ fifoFull

uint32_t MCAN_TxEventFifoStatus::fifoFull

Event FIFO Full
0 = Tx Event FIFO not full
1 = Tx Event FIFO full

§ eleLost

uint32_t MCAN_TxEventFifoStatus::eleLost

Tx Event FIFO Element Lost
0 = No Tx Event FIFO element lost
1 = Tx Event FIFO element lost, also set after write attempt to Tx Event FIFO of size zero.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale