58 #ifndef ti_drivers_aescbc_AESCBCLPF3__include 59 #define ti_drivers_aescbc_AESCBCLPF3__include 67 #include <ti/devices/DeviceFamily.h> 69 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) || (DeviceFamily_PARENT == DeviceFamily_PARENT_CC35XX) 73 #if (DeviceFamily_PARENT != DeviceFamily_PARENT_CC35XX) 74 #include DeviceFamily_constructPath(driverlib/aes.h) 105 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) || (DeviceFamily_PARENT == DeviceFamily_PARENT_CC35XX) 135 __STATIC_INLINE
bool AESCBC_acquireLock(
AESCBC_Handle handle, uint32_t timeout)
149 __STATIC_INLINE
void AESCBC_releaseLock(
AESCBC_Handle handle)
163 __STATIC_INLINE
void AESCBC_enableThreadSafety(
AESCBC_Handle handle)
166 object->threadSafe =
true;
181 __STATIC_INLINE
void AESCBC_disableThreadSafety(
AESCBC_Handle handle)
184 object->threadSafe =
false;
AESCBC_OperationUnion * operation
Definition: AESCBCLPF3.h:102
AESCommonLPF3_HWAttrs AESCBCLPF3_HWAttrs
AESCBCLPF3 Hardware Attributes.
Definition: AESCBCLPF3.h:87
bool CryptoResourceLPF3_acquireLock(uint32_t timeout)
bool threadSafe
Definition: AESCBCLPF3.h:104
const uint8_t * input
Definition: AESCBCLPF3.h:99
CryptoKeyKeyStore_PSA driver header.
AES Global configuration.
Definition: AESCommon.h:154
#define AES_IV_LENGTH_BYTES
Definition: AESCommonLPF3.h:92
AESCBC_CallbackFxn callbackFxn
Definition: AESCBCLPF3.h:101
int_fast16_t hsmStatus
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly.
Definition: AESCBCLPF3.h:112
AESCBC_OperationType operationType
Definition: AESCBCLPF3.h:103
size_t inputLength
Definition: AESCBCLPF3.h:106
uint32_t keyAssetID
Definition: AESCBCLPF3.h:113
AESCommonLPF3 Hardware Attributes.
Definition: AESCommonLPF3.h:103
bool segmentedOperationInProgress
Definition: AESCBCLPF3.h:117
psa_key_location_t KeyStore_PSA_KeyLocation
Definition: CryptoKeyKeyStore_PSA.h:251
void CryptoResourceLPF3_releaseLock(void)
KeyStore_PSA_KeyLocation keyLocation
Definition: AESCBCLPF3.h:114
AESCommon driver implementation for the Low Power F3 family.
Shared resources to arbitrate access to the AES engine.
AESCBC_OperationType
Enum for the operation types supported by the driver.
Definition: AESCBC.h:884
void * object
Definition: AESCommon.h:157
Union containing a reference to a one step or segmented operation.
Definition: AESCBC.h:875
AESCommonLPF3_Object common
Definition: AESCBCLPF3.h:97
AESCBCLPF3 Object.
Definition: AESCBCLPF3.h:94
uint8_t * output
Definition: AESCBCLPF3.h:100
void(* AESCBC_CallbackFxn)(AESCBC_Handle handle, int_fast16_t returnValue, AESCBC_OperationUnion *operation, AESCBC_OperationType operationType)
The definition of a callback function used by the AESCBC driver when used in AESCBC_RETURN_BEHAVIOR_C...
Definition: AESCBC.h:912
AESCommonLPF3 Object.
Definition: AESCommonLPF3.h:125