Macros | Typedefs | Functions
CryptoKeyKeyStore_PSA.h File Reference

Detailed Description

CryptoKeyKeyStore_PSA driver header.

============================================================================

Warning
This is a beta API. It may change in future releases.

Overview

This file contains the APIs to import, export, copy, and destroy key store CryptoKeys. Key store CryptoKeys reference keying material stored in flash or RAM using a key identifier. These CryptoKeys are subject to enforced usage restrictions as defined by the key attributes assigned during key import. This file provides definitions that are common between the Non-Secure Processing Environment (NSPE) and Secure Processing Environment (SPE).

Usage

After calling the key store initialization function, a CryptoKey must be imported into the key store before it can be used for a crypto operation APIs which takes a CryptoKey as an input.

Importing and destroying a persistent AES-CCM KeyStore key

....
uint8_t keyingMaterial[16] = {0x1f, 0x8e, 0x49, 0x73, 0x95, 0x3f, 0x3f, 0xb0,
0xbd, 0x6b, 0x16, 0x66, 0x2e, 0x9a, 0x3c, 0x17};
CryptoKey cryptoKey;
int_fast16_t status;
// Assign key attributes
// Set key ID
KeyStore_PSA_setKeyId(&attributes, keyID);
// Import the keyingMaterial
status = KeyStore_PSA_importKey(&attributes, keyingMaterial, sizeof(keyingMaterial), &keyID);
{
// Handle error
}
// Initialize cryptoKey for crypto operations
KeyStore_PSA_initKey(&cryptoKey, keyID, sizeof(keyingMaterial), NULL);
// Use the cryptoKey for AESCCM operations
// Destroy key after use
status = KeyStore_PSA_destroyKey(keyID);
{
// Handle error
}
#include <ti/devices/DeviceFamily.h>
#include <third_party/hsmddk/include/Integration/Adapter_PSA/incl/psa/crypto.h>
#include <third_party/hsmddk/include/Integration/Adapter_PSA/incl/psa/crypto_extra.h>
#include <third_party/hsmddk/include/Integration/Adapter_PSA/Adapter_mbedTLS/incl/private_access.h>
Include dependency graph for CryptoKeyKeyStore_PSA.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Macros

#define KEYSTORE_PSA_STATUS_SUCCESS   ((int_fast16_t)PSA_SUCCESS)
 
#define KEYSTORE_PSA_STATUS_GENERIC_ERROR   ((int_fast16_t)PSA_ERROR_GENERIC_ERROR)
 
#define KEYSTORE_PSA_STATUS_NOT_SUPPORTED   ((int_fast16_t)PSA_ERROR_NOT_SUPPORTED)
 
#define KEYSTORE_PSA_STATUS_NOT_PERMITTED   ((int_fast16_t)PSA_ERROR_NOT_PERMITTED)
 
#define KEYSTORE_PSA_STATUS_INVALID_KEY_ID   ((int_fast16_t)PSA_ERROR_INVALID_HANDLE)
 
#define KEYSTORE_PSA_STATUS_BUFFER_TOO_SMALL   ((int_fast16_t)PSA_ERROR_BUFFER_TOO_SMALL)
 
#define KEYSTORE_PSA_STATUS_ALREADY_EXISTS   ((int_fast16_t)PSA_ERROR_ALREADY_EXISTS)
 
#define KEYSTORE_PSA_STATUS_DOES_NOT_EXIST   ((int_fast16_t)PSA_ERROR_DOES_NOT_EXIST)
 
#define KEYSTORE_PSA_STATUS_BAD_STATE   ((int_fast16_t)PSA_ERROR_BAD_STATE)
 
#define KEYSTORE_PSA_STATUS_INVALID_ARGUMENT   ((int_fast16_t)PSA_ERROR_INVALID_ARGUMENT)
 
#define KEYSTORE_PSA_STATUS_INSUFFICIENT_MEMORY   ((int_fast16_t)PSA_ERROR_INSUFFICIENT_MEMORY)
 
#define KEYSTORE_PSA_STATUS_INSUFFICIENT_STORAGE   ((int_fast16_t)PSA_ERROR_INSUFFICIENT_STORAGE)
 
#define KEYSTORE_PSA_STATUS_COMMUNICATION_FAILURE   ((int_fast16_t)PSA_ERROR_COMMUNICATION_FAILURE)
 
#define KEYSTORE_PSA_STATUS_STORAGE_FAILURE   ((int_fast16_t)PSA_ERROR_STORAGE_FAILURE)
 
#define KEYSTORE_PSA_STATUS_HARDWARE_FAILURE   ((int_fast16_t)PSA_ERROR_HARDWARE_FAILURE)
 
#define KEYSTORE_PSA_STATUS_INSUFFICIENT_ENTROPY   ((int_fast16_t)PSA_ERROR_INSUFFICIENT_ENTROPY)
 
#define KEYSTORE_PSA_STATUS_CORRUPTION_DETECTED   ((int_fast16_t)PSA_ERROR_CORRUPTION_DETECTED)
 
#define KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLE   ((int_fast16_t)-250)
 An error status code returned if the hardware or software resource is currently unavailable. More...
 
#define KEYSTORE_PSA_KEY_TYPE_RAW_DATA   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_RAW_DATA)
 
#define KEYSTORE_PSA_KEY_TYPE_HMAC   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_HMAC)
 
#define KEYSTORE_PSA_KEY_TYPE_DERIVE   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_DERIVE)
 
#define KEYSTORE_PSA_KEY_TYPE_AES   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_AES)
 
#define KEYSTORE_PSA_KEY_TYPE_DES   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_DES)
 
#define KEYSTORE_PSA_KEY_TYPE_CAMELLIA   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_CAMELLIA)
 
#define KEYSTORE_PSA_KEY_TYPE_ARC4   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_ARC4)
 
#define KEYSTORE_PSA_KEY_TYPE_CHACHA20   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_CHACHA20)
 
#define KEYSTORE_PSA_KEY_TYPE_RSA_PUBLIC_KEY   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_RSA_PUBLIC_KEY)
 
#define KEYSTORE_PSA_KEY_TYPE_RSA_KEY_PAIR   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_RSA_KEY_PAIR)
 
#define PSA_KEY_TYPE_IS_RSA(type)   (PSA_KEY_TYPE_PUBLIC_KEY_OF_KEY_PAIR(type) == PSA_KEY_TYPE_RSA_PUBLIC_KEY)
 
#define KEYSTORE_PSA_KEY_TYPE_ECC_PUBLIC_KEY_BASE   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_ECC_PUBLIC_KEY_BASE)
 
#define KEYSTORE_PSA_KEY_TYPE_ECC_KEY_PAIR_BASE   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_ECC_KEY_PAIR_BASE)
 
#define KEYSTORE_PSA_KEY_TYPE_PASSWORD   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_PASSWORD)
 
#define KEYSTORE_PSA_KEY_TYPE_PASSWORD_HASH   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_PASSWORD_HASH)
 
#define KEYSTORE_PSA_ALG_SHA_224   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_224)
 
#define KEYSTORE_PSA_ALG_SHA_256   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_256)
 
#define KEYSTORE_PSA_ALG_SHA_384   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_384)
 
#define KEYSTORE_PSA_ALG_SHA_512   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_512)
 
#define KEYSTORE_PSA_ALG_SHA_512_224   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_512_224)
 
#define KEYSTORE_PSA_ALG_SHA_512_256   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_512_256)
 
#define KEYSTORE_PSA_ALG_HMAC(hash_alg)   ((KeyStore_PSA_Algorithm)(PSA_ALG_HMAC(hash_alg)))
 
#define KEYSTORE_PSA_ALG_CBC_MAC   ((KeyStore_PSA_Algorithm)PSA_ALG_CBC_MAC)
 
#define KEYSTORE_PSA_ALG_CMAC   ((KeyStore_PSA_Algorithm)PSA_ALG_CMAC)
 
#define KEYSTORE_PSA_ALG_CTR   ((KeyStore_PSA_Algorithm)PSA_ALG_CTR)
 
#define KEYSTORE_PSA_ALG_ECB_NO_PADDING   ((KeyStore_PSA_Algorithm)PSA_ALG_ECB_NO_PADDING)
 
#define KEYSTORE_PSA_ALG_CBC_NO_PADDING   ((KeyStore_PSA_Algorithm)PSA_ALG_CBC_NO_PADDING)
 
#define KEYSTORE_PSA_ALG_CCM   ((KeyStore_PSA_Algorithm)PSA_ALG_CCM)
 
#define KEYSTORE_PSA_ALG_GCM   ((KeyStore_PSA_Algorithm)PSA_ALG_GCM)
 
#define KEYSTORE_PSA_ALG_CHACHA20_POLY1305   ((KeyStore_PSA_Algorithm)PSA_ALG_CHACHA20_POLY1305)
 
#define KEYSTORE_PSA_ALG_ECDH   ((KeyStore_PSA_Algorithm)PSA_ALG_ECDH)
 
#define KEYSTORE_PSA_ALG_ECDSA   ((KeyStore_PSA_Algorithm)PSA_ALG_ECDSA_ANY)
 
#define KEYSTORE_PSA_ALG_PAKE   ((KeyStore_PSA_Algorithm)PSA_ALG_JPAKE)
 
#define KEYSTORE_PSA_ALG_PURE_EDDSA   ((KeyStore_PSA_Algorithm)PSA_ALG_PURE_EDDSA)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT163K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT163R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT163R2   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R2)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT193R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT193R2   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R2)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT233K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT233R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT239K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT283K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT283R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT409K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT409R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT571K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECT571R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP160K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP160R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP160R2   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R2)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP192K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP192R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP224K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP224R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP256K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP256R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP384R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_SECP521R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)
 
#define KEYSTORE_ECC_CURVE_BRAINPOOL_P256R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_BRAINPOOL_P_R1)
 
#define KEYSTORE_ECC_CURVE_BRAINPOOL_P384R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_BRAINPOOL_P_R1)
 
#define KEYSTORE_ECC_CURVE_BRAINPOOL_P512R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_BRAINPOOL_P_R1)
 
#define KEYSTORE_PSA_ECC_CURVE_ED25519   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_TWISTED_EDWARDS)
 
#define KEYSTORE_PSA_ECC_CURVE_CURVE25519   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_MONTGOMERY)
 
#define KEYSTORE_PSA_ECC_CURVE_CURVE448   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_MONTGOMERY)
 
#define KEYSTORE_PSA_ECC_CURVE_VENDOR_MIN   ((KeyStore_PSA_KeyType)PSA_ECC_CURVE_VENDOR_MIN)
 
#define KEYSTORE_PSA_ECC_CURVE_VENDOR_MAX   ((KeyStore_PSA_KeyType)PSA_ECC_CURVE_VENDOR_MAX)
 
#define KEYSTORE_PSA_MIN_VOLATILE_KEY_ID   PSA_KEY_ID_VOLATILE_MIN
 
#define KEYSTORE_PSA_MAX_VOLATILE_KEY_ID   PSA_KEY_ID_VOLATILE_MAX
 
#define MEMBER_SIZE(type, member)   sizeof(((type *)0)->member)
 
#define KEYSTORE_PSA_KEY_LIFETIME_VOLATILE   ((KeyStore_PSA_KeyLifetime)PSA_KEY_LIFETIME_VOLATILE)
 
#define KEYSTORE_PSA_KEY_LIFETIME_PERSISTENT   ((KeyStore_PSA_KeyLifetime)PSA_KEY_LIFETIME_PERSISTENT)
 
#define KEYSTORE_PSA_KEY_PERSISTENCE_VOLATILE   ((KeyStore_PSA_KeyPersistence)PSA_KEY_PERSISTENCE_VOLATILE)
 
#define KEYSTORE_PSA_KEY_PERSISTENCE_DEFAULT   ((KeyStore_PSA_KeyPersistence)PSA_KEY_PERSISTENCE_DEFAULT)
 
#define KEYSTORE_PSA_KEY_PERSISTENCE_HSM_ASSET_STORE   ((KeyStore_PSA_KeyPersistence)0x80U)
 
#define KEYSTORE_PSA_KEY_PERSISTENCE_READ_ONLY   ((KeyStore_PSA_KeyPersistence)PSA_KEY_PERSISTENCE_READ_ONLY)
 
#define KEYSTORE_PSA_KEY_LIFETIME_GET_PERSISTENCE(lifetime)   ((KeyStore_PSA_KeyPersistence)((lifetime) & 0x000000ff))
 
#define KEYSTORE_PSA_KEY_LIFETIME_GET_LOCATION(lifetime)   ((KeyStore_PSA_KeyLocation)((lifetime) >> 8))
 
#define KEYSTORE_PSA_KEY_LIFETIME_IS_VOLATILE(lifetime)   (KEYSTORE_PSA_KEY_LIFETIME_GET_PERSISTENCE(lifetime) == KEYSTORE_PSA_KEY_PERSISTENCE_VOLATILE)
 
#define KEYSTORE_PSA_KEY_LIFETIME_IS_READ_ONLY(lifetime)   (KEYSTORE_PSA_KEY_LIFETIME_GET_PERSISTENCE(lifetime) == KEYSTORE_PSA_KEY_PERSISTENCE_READ_ONLY)
 
#define KEYSTORE_PSA_KEY_LIFETIME_FROM_PERSISTENCE_AND_LOCATION(persistence, location)   (PSA_KEY_LIFETIME_FROM_PERSISTENCE_AND_LOCATION(persistence, location))
 
#define KEYSTORE_PSA_KEY_LOCATION_LOCAL_STORAGE   ((KeyStore_PSA_KeyLocation)PSA_KEY_LOCATION_LOCAL_STORAGE)
 
#define KEYSTORE_PSA_KEY_LOCATION_HSM_ASSET_STORE   ((KeyStore_PSA_KeyLocation)0x000001U)
 
#define KEYSTORE_PSA_KEY_ID_NULL   ((KeyStore_PSA_keyID)0x0)
 
#define KEYSTORE_PSA_KEY_ID_USER_MAX   ((KeyStore_PSA_keyID)PSA_KEY_ID_USER_MAX)
 
#define KEYSTORE_PSA_KEY_ID_USER_MIN   ((KeyStore_PSA_keyID)PSA_KEY_ID_USER_MIN)
 
#define KEYSTORE_PSA_KEY_ID_USER_MAX   ((KeyStore_PSA_keyID)PSA_KEY_ID_USER_MAX)
 
#define KEYSTORE_PSA_KEY_ID_VENDOR_MIN   ((KeyStore_PSA_keyID)PSA_KEY_ID_VENDOR_MIN)
 
#define KEYSTORE_PSA_KEY_ID_VENDOR_MAX   ((KeyStore_PSA_keyID)PSA_KEY_ID_VENDOR_MAX)
 
#define KEYSTORE_PSA_DEFAULT_OWNER   MBEDTLS_PSA_CRYPTO_KEY_ID_DEFAULT_OWNER
 
#define KEYSTORE_PSA_KEY_USAGE_EXPORT   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_EXPORT)
 
#define KEYSTORE_PSA_KEY_USAGE_COPY   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_COPY)
 
#define KEYSTORE_PSA_KEY_USAGE_ENCRYPT   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_ENCRYPT)
 
#define KEYSTORE_PSA_KEY_USAGE_DECRYPT   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_DECRYPT)
 
#define KEYSTORE_PSA_KEY_USAGE_SIGN_MESSAGE   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_SIGN_MESSAGE)
 
#define KEYSTORE_PSA_KEY_USAGE_VERIFY_MESSAGE   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_VERIFY_MESSAGE)
 
#define KEYSTORE_PSA_KEY_USAGE_SIGN_HASH   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_SIGN_HASH)
 
#define KEYSTORE_PSA_KEY_USAGE_VERIFY_HASH   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_VERIFY_HASH)
 
#define KEYSTORE_PSA_KEY_USAGE_DERIVE   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_DERIVE)
 
#define KEYSTORE_PSA_KEY_ATTRIBUTES_INIT   PSA_KEY_ATTRIBUTES_INIT
 
#define GET_KEY_ID(keyID, ID)   keyID = ID
 
#define SET_KEY_ID(ID, keyID)   ID = keyID
 
#define KEYSTORE_PSA_PREPROVISIONED_AREA_ADDR   0x0000
 
#define KEYSTORE_PSA_PREPROVISIONED_AREA_SIZE   (0x700) /* 1792 B */
 Area size for pre-provisioned keys, 2KB - 256B (reserved for attestation data) More...
 
#define KEYSTORE_PSA_PREPROVISIONED_KEYS_EMPTY   0xFFFF
 Macro to indicate empty pre-provisioned key memory. More...
 
#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_MAGIC_HEADER   "HUK\0KEY"
 Pre-provisioned key storage magic header. More...
 
#define KEYSTORE_PSA_PRE_PROVISIONED_KEYS_END   0
 
#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_MAGIC_HEADER_LENGTH   (sizeof(KEYSTORE_PSA_PRE_PROVISIONED_KEY_MAGIC_HEADER))
 
#define KEYSTORE_PSA_PRE_PROVISIONED_KEYS_END_LENGTH   (sizeof(KEYSTORE_PSA_PRE_PROVISIONED_KEYS_END))
 
#define KEYSTORE_PSA_MAX_PREPROVISIONED_KEYS   0x10
 
#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_VALID_LIFETIME   0xAAAA
 Pre-provisioned key Lifetime. More...
 
#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_INVALID_LIFETIME   0x8888
 
#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_ID_MAX   MBEDTLS_PSA_KEY_ID_BUILTIN_MAX
 Admissible key ID range for Pre-provisioned keys. More...
 
#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_ID_MIN   MBEDTLS_PSA_KEY_ID_BUILTIN_MIN
 

Typedefs

typedef psa_key_usage_t KeyStore_PSA_KeyUsage
 Encoding of permitted usage on a key. More...
 
typedef psa_key_lifetime_t KeyStore_PSA_KeyLifetime
 
typedef psa_key_persistence_t KeyStore_PSA_KeyPersistence
 
typedef psa_key_location_t KeyStore_PSA_KeyLocation
 
typedef psa_key_type_t KeyStore_PSA_KeyType
 Encoding of a key type. More...
 
typedef psa_algorithm_t KeyStore_PSA_Algorithm
 Encoding of a cryptographic algorithm. More...
 
typedef psa_key_attributes_t KeyStore_PSA_KeyAttributes
 
typedef mbedtls_svc_key_id_t KeyStore_PSA_KeyFileId
 

Functions

void KeyStore_PSA_setKeyId (KeyStore_PSA_KeyAttributes *attributes, KeyStore_PSA_KeyFileId key)
 Declare a key as persistent and set its key identifier. More...
 
void KeyStore_PSA_setKeyLifetime (KeyStore_PSA_KeyAttributes *attributes, KeyStore_PSA_KeyLifetime lifetime)
 Set the location of a persistent key. More...
 
KeyStore_PSA_KeyFileId KeyStore_PSA_getKeyId (KeyStore_PSA_KeyAttributes *attributes)
 Retrieve the key identifier from key attributes. More...
 
KeyStore_PSA_KeyLifetime KeyStore_PSA_getKeyLifetime (KeyStore_PSA_KeyAttributes *attributes)
 Retrieve the lifetime from key attributes. More...
 
void KeyStore_PSA_setKeyUsageFlags (KeyStore_PSA_KeyAttributes *attributes, KeyStore_PSA_KeyUsage usageFlags)
 Declare usage flags for a key. More...
 
KeyStore_PSA_KeyUsage KeyStore_PSA_getKeyUsageFlags (KeyStore_PSA_KeyAttributes *attributes)
 Retrieve the usage flags from key attributes. More...
 
void KeyStore_PSA_setKeyAlgorithm (KeyStore_PSA_KeyAttributes *attributes, KeyStore_PSA_Algorithm alg)
 Declare the permitted algorithm policy for a key. More...
 
KeyStore_PSA_Algorithm KeyStore_PSA_getKeyAlgorithm (KeyStore_PSA_KeyAttributes *attributes)
 Retrieve the algorithm policy from key attributes. More...
 
void KeyStore_PSA_setKeyType (KeyStore_PSA_KeyAttributes *attributes, KeyStore_PSA_KeyType type)
 Declare the type of a key. More...
 
void KeyStore_PSA_setKeyBits (KeyStore_PSA_KeyAttributes *attributes, size_t bits)
 Declare the size of a key. More...
 
KeyStore_PSA_KeyType KeyStore_PSA_getKeyType (KeyStore_PSA_KeyAttributes *attributes)
 Retrieve the key type from key attributes. More...
 
size_t KeyStore_PSA_getKeyBits (KeyStore_PSA_KeyAttributes *attributes)
 Retrieve the key size from key attributes. More...
 
void KeyStore_PSA_resetKeyAttributes (KeyStore_PSA_KeyAttributes *attributes)
 Reset a key attribute structure to a freshly initialized state. More...
 
int_fast16_t KeyStore_PSA_exportPublicKey (KeyStore_PSA_KeyFileId key, uint8_t *data, size_t dataSize, size_t *dataLength)
 Export a public key or the public part of a key pair in binary format. More...
 
int_fast16_t KeyStore_PSA_exportKey (KeyStore_PSA_KeyFileId key, uint8_t *data, size_t dataSize, size_t *dataLength)
 Export a key in binary format. More...
 
int_fast16_t KeyStore_PSA_importKey (KeyStore_PSA_KeyAttributes *attributes, uint8_t *data, size_t dataLength, KeyStore_PSA_KeyFileId *key)
 Import a key in binary format. More...
 
int_fast16_t KeyStore_PSA_getKeyAttributes (KeyStore_PSA_KeyFileId key, KeyStore_PSA_KeyAttributes *attributes)
 Retrieve the attributes of a key. More...
 
int_fast16_t KeyStore_PSA_purgeKey (KeyStore_PSA_KeyFileId key)
 Remove non-essential copies of key material from memory. More...
 
int_fast16_t KeyStore_PSA_destroyKey (KeyStore_PSA_KeyFileId key)
 Destroy a key. More...
 
int_fast16_t KeyStore_PSA_copyKey (KeyStore_PSA_KeyFileId source_key, KeyStore_PSA_KeyAttributes *attributes, KeyStore_PSA_KeyFileId *target_key)
 Make a copy of a key. More...
 

Macro Definition Documentation

§ KEYSTORE_PSA_STATUS_SUCCESS

#define KEYSTORE_PSA_STATUS_SUCCESS   ((int_fast16_t)PSA_SUCCESS)

The action was completed successfully.

§ KEYSTORE_PSA_STATUS_GENERIC_ERROR

#define KEYSTORE_PSA_STATUS_GENERIC_ERROR   ((int_fast16_t)PSA_ERROR_GENERIC_ERROR)

An error occurred that does not correspond to any defined failure cause.

Implementations may use this error code if none of the other standard error codes are applicable.

§ KEYSTORE_PSA_STATUS_NOT_SUPPORTED

#define KEYSTORE_PSA_STATUS_NOT_SUPPORTED   ((int_fast16_t)PSA_ERROR_NOT_SUPPORTED)

The requested operation or a parameter is not supported by this implementation.

Implementations should return this error code when an enumeration parameter such as a key type, algorithm, etc. is not recognized. If a combination of parameters is recognized and identified as not valid, return KEYSTORE_PSA_STATUS_INVALID_ARGUMENT instead.

§ KEYSTORE_PSA_STATUS_NOT_PERMITTED

#define KEYSTORE_PSA_STATUS_NOT_PERMITTED   ((int_fast16_t)PSA_ERROR_NOT_PERMITTED)

The requested action is denied by a policy.

Implementations should return this error code when the parameters are recognized as valid and supported, and a policy explicitly denies the requested operation.

If a subset of the parameters of a function call identify a forbidden operation, and another subset of the parameters are not valid or not supported, it is unspecified whether the function returns KEYSTORE_PSA_STATUS_NOT_PERMITTED, KEYSTORE_PSA_STATUS_NOT_SUPPORTED or KEYSTORE_PSA_STATUS_INVALID_ARGUMENT.

§ KEYSTORE_PSA_STATUS_INVALID_KEY_ID

#define KEYSTORE_PSA_STATUS_INVALID_KEY_ID   ((int_fast16_t)PSA_ERROR_INVALID_HANDLE)

The key ID is not valid or does not exist.

§ KEYSTORE_PSA_STATUS_BUFFER_TOO_SMALL

#define KEYSTORE_PSA_STATUS_BUFFER_TOO_SMALL   ((int_fast16_t)PSA_ERROR_BUFFER_TOO_SMALL)

An output buffer is too small.

Applications can call the PSA_xxx_SIZE macro listed in the function description to determine a sufficient buffer size.

Implementations should preferably return this error code only in cases when performing the operation with a larger output buffer would succeed. However implementations may return this error if a function has invalid or unsupported parameters in addition to the parameters that determine the necessary output buffer size.

§ KEYSTORE_PSA_STATUS_ALREADY_EXISTS

#define KEYSTORE_PSA_STATUS_ALREADY_EXISTS   ((int_fast16_t)PSA_ERROR_ALREADY_EXISTS)

Asking for an item that already exists

Implementations should return this error, when attempting to write an item (like a key) that already exists.

§ KEYSTORE_PSA_STATUS_DOES_NOT_EXIST

#define KEYSTORE_PSA_STATUS_DOES_NOT_EXIST   ((int_fast16_t)PSA_ERROR_DOES_NOT_EXIST)

Asking for an item that doesn't exist

Implementations should return this error, if a requested item (like a key) does not exist.

§ KEYSTORE_PSA_STATUS_BAD_STATE

#define KEYSTORE_PSA_STATUS_BAD_STATE   ((int_fast16_t)PSA_ERROR_BAD_STATE)

The requested action cannot be performed in the current state.

Multipart operations return this error when one of the functions is called out of sequence. Refer to the function descriptions for permitted sequencing of functions.

Implementations shall not return this error code to indicate that a key either exists or not, but shall instead return KEYSTORE_PSA_STATUS_ALREADY_EXISTS or KEYSTORE_PSA_STATUS_DOES_NOT_EXIST as applicable.

Implementations shall not return this error code to indicate that a key ID is invalid, but shall return KEYSTORE_PSA_STATUS_INVALID_KEY_ID instead.

§ KEYSTORE_PSA_STATUS_INVALID_ARGUMENT

#define KEYSTORE_PSA_STATUS_INVALID_ARGUMENT   ((int_fast16_t)PSA_ERROR_INVALID_ARGUMENT)

The parameters passed to the function are invalid.

Implementations may return this error any time a parameter or combination of parameters are recognized as invalid.

Implementations shall not return this error code to indicate that a key ID is invalid, but shall return KEYSTORE_PSA_STATUS_INVALID_KEY_ID instead.

§ KEYSTORE_PSA_STATUS_INSUFFICIENT_MEMORY

#define KEYSTORE_PSA_STATUS_INSUFFICIENT_MEMORY   ((int_fast16_t)PSA_ERROR_INSUFFICIENT_MEMORY)

There is not enough runtime memory.

If the action is carried out across multiple security realms, this error can refer to available memory in any of the security realms.

§ KEYSTORE_PSA_STATUS_INSUFFICIENT_STORAGE

#define KEYSTORE_PSA_STATUS_INSUFFICIENT_STORAGE   ((int_fast16_t)PSA_ERROR_INSUFFICIENT_STORAGE)

There is not enough persistent storage.

Functions that modify the key storage return this error code if there is insufficient storage space on the host media. In addition, many functions that do not otherwise access storage may return this error code if the implementation requires a mandatory log entry for the requested action and the log storage space is full.

§ KEYSTORE_PSA_STATUS_COMMUNICATION_FAILURE

#define KEYSTORE_PSA_STATUS_COMMUNICATION_FAILURE   ((int_fast16_t)PSA_ERROR_COMMUNICATION_FAILURE)

There was a communication failure inside the implementation.

This can indicate a communication failure between the application and an external cryptoprocessor or between the cryptoprocessor and an external volatile or persistent memory. A communication failure may be transient or permanent depending on the cause.

Warning
If a function returns this error, it is undetermined whether the requested action has completed or not. Implementations should return KEYSTORE_PSA_STATUS_SUCCESS on successful completion whenever possible, however functions may return KEYSTORE_PSA_STATUS_COMMUNICATION_FAILURE if the requested action was completed successfully in an external cryptoprocessor but there was a breakdown of communication before the cryptoprocessor could report the status to the application.

§ KEYSTORE_PSA_STATUS_STORAGE_FAILURE

#define KEYSTORE_PSA_STATUS_STORAGE_FAILURE   ((int_fast16_t)PSA_ERROR_STORAGE_FAILURE)

There was a storage failure that may have led to data loss.

This error indicates that some persistent storage is corrupted. It should not be used for a corruption of volatile memory (use KEYSTORE_PSA_STATUS_CORRUPTION_DETECTED), for a communication error between the cryptoprocessor and its external storage (use KEYSTORE_PSA_STATUS_COMMUNICATION_FAILURE), or when the storage is in a valid state but is full (use KEYSTORE_PSA_STATUS_INSUFFICIENT_STORAGE).

Note that a storage failure does not indicate that any data that was previously read is invalid. However this previously read data may no longer be readable from storage.

When a storage failure occurs, it is no longer possible to ensure the global integrity of the keystore. Depending on the global integrity guarantees offered by the implementation, access to other data may or may not fail even if the data is still readable but its integrity cannot be guaranteed.

Implementations should only use this error code to report a permanent storage corruption. However application writers should keep in mind that transient errors while reading the storage may be reported using this error code.

§ KEYSTORE_PSA_STATUS_HARDWARE_FAILURE

#define KEYSTORE_PSA_STATUS_HARDWARE_FAILURE   ((int_fast16_t)PSA_ERROR_HARDWARE_FAILURE)

A hardware failure was detected.

A hardware failure may be transient or permanent depending on the cause.

§ KEYSTORE_PSA_STATUS_INSUFFICIENT_ENTROPY

#define KEYSTORE_PSA_STATUS_INSUFFICIENT_ENTROPY   ((int_fast16_t)PSA_ERROR_INSUFFICIENT_ENTROPY)

There is not enough entropy to generate random data needed for the requested action.

This error indicates a failure of a hardware random generator. Application writers should note that this error can be returned not only by functions whose purpose is to generate random data, such as key, IV or nonce generation, but also by functions that execute an algorithm with a randomized result, as well as functions that use randomization of intermediate computations as a countermeasure to certain attacks.

Implementations should avoid returning this error after KeyStore_PSA_init() has succeeded. Implementations should generate sufficient entropy during initialization and subsequently use a cryptographically secure pseudorandom generator (PRNG). However implementations may return this error at any time if a policy requires the PRNG to be reseeded during normal operation.

§ KEYSTORE_PSA_STATUS_CORRUPTION_DETECTED

#define KEYSTORE_PSA_STATUS_CORRUPTION_DETECTED   ((int_fast16_t)PSA_ERROR_CORRUPTION_DETECTED)

A tampering attempt was detected.

If an application receives this error code, there is no guarantee that previously accessed or computed data was correct and remains confidential. Applications should not perform any security function and should enter a safe failure state.

Implementations may return this error code if they detect an invalid state that cannot happen during normal operation and that indicates that the implementation's security guarantees no longer hold. Depending on the implementation architecture and on its security and safety goals, the implementation may forcibly terminate the application.

This error code is intended as a last resort when a security breach is detected and it is unsure whether the keystore data is still protected. Implementations shall only return this error code to report an alarm from a tampering detector, to indicate that the confidentiality of stored data can no longer be guaranteed, or to indicate that the integrity of previously returned data is now considered compromised. Implementations shall not use this error code to indicate a hardware failure that merely makes it impossible to perform the requested operation (use KEYSTORE_PSA_STATUS_COMMUNICATION_FAILURE, KEYSTORE_PSA_STATUS_STORAGE_FAILURE, KEYSTORE_PSA_STATUS_HARDWARE_FAILURE or other applicable error code instead).

This error indicates an attack against the application. Implementations shall not return this error code as a consequence of the behavior of the application itself.

§ KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLE

#define KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLE   ((int_fast16_t)-250)

An error status code returned if the hardware or software resource is currently unavailable.

KeyStore driver implementation may have limitations on how many clients can simultaneously perform operations on the same key. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

§ KEYSTORE_PSA_KEY_TYPE_RAW_DATA

#define KEYSTORE_PSA_KEY_TYPE_RAW_DATA   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_RAW_DATA)

Raw data.

A "key" of this type cannot be used for any cryptographic operation. Applications may use this type to store arbitrary data in the keystore.

§ KEYSTORE_PSA_KEY_TYPE_HMAC

#define KEYSTORE_PSA_KEY_TYPE_HMAC   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_HMAC)

HMAC key.

The key policy determines which underlying hash algorithm the key can be used for.

HMAC keys should generally have the same size as the underlying hash.

§ KEYSTORE_PSA_KEY_TYPE_DERIVE

#define KEYSTORE_PSA_KEY_TYPE_DERIVE   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_DERIVE)

A secret for key derivation.

The key policy determines which key derivation algorithm the key can be used for.

§ KEYSTORE_PSA_KEY_TYPE_AES

#define KEYSTORE_PSA_KEY_TYPE_AES   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_AES)

Key for a cipher, AEAD or MAC algorithm based on the AES block cipher.

The size of the key can be 16 bytes (AES-128), 24 bytes (AES-192) or 32 bytes (AES-256).

§ KEYSTORE_PSA_KEY_TYPE_DES

#define KEYSTORE_PSA_KEY_TYPE_DES   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_DES)

Key for a cipher or MAC algorithm based on DES or 3DES (Triple-DES).

The size of the key can be 64 bits (single DES), 128 bits (2-key 3DES) or 192 bits (3-key 3DES).

Note that single DES and 2-key 3DES are weak and strongly deprecated and should only be used to decrypt legacy data. 3-key 3DES is weak and deprecated and should only be used in legacy protocols.

§ KEYSTORE_PSA_KEY_TYPE_CAMELLIA

#define KEYSTORE_PSA_KEY_TYPE_CAMELLIA   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_CAMELLIA)

Key for a cipher, AEAD or MAC algorithm based on the Camellia block cipher.

§ KEYSTORE_PSA_KEY_TYPE_ARC4

#define KEYSTORE_PSA_KEY_TYPE_ARC4   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_ARC4)

Key for the RC4 stream cipher.

Note that RC4 is weak and deprecated and should only be used in legacy protocols.

§ KEYSTORE_PSA_KEY_TYPE_CHACHA20

#define KEYSTORE_PSA_KEY_TYPE_CHACHA20   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_CHACHA20)

Key for the ChaCha20 stream cipher or the Chacha20-Poly1305 AEAD algorithm.

ChaCha20 and the ChaCha20_Poly1305 construction are defined in RFC 7539.

Implementations must support 12-byte nonces, may support 8-byte nonces, and should reject other sizes.

§ KEYSTORE_PSA_KEY_TYPE_RSA_PUBLIC_KEY

#define KEYSTORE_PSA_KEY_TYPE_RSA_PUBLIC_KEY   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_RSA_PUBLIC_KEY)

RSA public key.

The size of an RSA key is the bit size of the modulus.

§ KEYSTORE_PSA_KEY_TYPE_RSA_KEY_PAIR

#define KEYSTORE_PSA_KEY_TYPE_RSA_KEY_PAIR   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_RSA_KEY_PAIR)

RSA key pair (private and public key).

The size of an RSA key is the bit size of the modulus.

§ PSA_KEY_TYPE_IS_RSA

#define PSA_KEY_TYPE_IS_RSA (   type)    (PSA_KEY_TYPE_PUBLIC_KEY_OF_KEY_PAIR(type) == PSA_KEY_TYPE_RSA_PUBLIC_KEY)

Whether a key type is an RSA key (pair or public-only).

§ KEYSTORE_PSA_KEY_TYPE_ECC_PUBLIC_KEY_BASE

#define KEYSTORE_PSA_KEY_TYPE_ECC_PUBLIC_KEY_BASE   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_ECC_PUBLIC_KEY_BASE)

§ KEYSTORE_PSA_KEY_TYPE_ECC_KEY_PAIR_BASE

#define KEYSTORE_PSA_KEY_TYPE_ECC_KEY_PAIR_BASE   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_ECC_KEY_PAIR_BASE)

§ KEYSTORE_PSA_KEY_TYPE_PASSWORD

#define KEYSTORE_PSA_KEY_TYPE_PASSWORD   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_PASSWORD)

A low-entropy secret for password hashing or key derivation.

This key type is suitable for passwords and passphrases which are typically intended to be memorizable by humans, and have a low entropy relative to their size. It can be used for randomly generated or derived keys with maximum or near-maximum entropy, but KEYSTORE_PSA_KEY_TYPE_PASSWORD is more suitable for such keys. It is not suitable for passwords with extremely low entropy, such as numerical PINs.

The key policy determines which key derivation algorithm the key can be used for.

§ KEYSTORE_PSA_KEY_TYPE_PASSWORD_HASH

#define KEYSTORE_PSA_KEY_TYPE_PASSWORD_HASH   ((KeyStore_PSA_KeyType)PSA_KEY_TYPE_PASSWORD_HASH)

A secret value that can be used to verify a password hash.

The key policy determines which key derivation algorithm the key can be used for, among the same permissible subset as for KEYSTORE_PSA_KEY_TYPE_PASSWORD.

§ KEYSTORE_PSA_ALG_SHA_224

#define KEYSTORE_PSA_ALG_SHA_224   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_224)

SHA2-224

§ KEYSTORE_PSA_ALG_SHA_256

#define KEYSTORE_PSA_ALG_SHA_256   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_256)

SHA2-256

§ KEYSTORE_PSA_ALG_SHA_384

#define KEYSTORE_PSA_ALG_SHA_384   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_384)

SHA2-384

§ KEYSTORE_PSA_ALG_SHA_512

#define KEYSTORE_PSA_ALG_SHA_512   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_512)

SHA2-512

§ KEYSTORE_PSA_ALG_SHA_512_224

#define KEYSTORE_PSA_ALG_SHA_512_224   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_512_224)

SHA2-512/224

§ KEYSTORE_PSA_ALG_SHA_512_256

#define KEYSTORE_PSA_ALG_SHA_512_256   ((KeyStore_PSA_Algorithm)PSA_ALG_SHA_512_256)

SHA2-512/256

§ KEYSTORE_PSA_ALG_HMAC

#define KEYSTORE_PSA_ALG_HMAC (   hash_alg)    ((KeyStore_PSA_Algorithm)(PSA_ALG_HMAC(hash_alg)))

Macro to build an HMAC algorithm

§ KEYSTORE_PSA_ALG_CBC_MAC

#define KEYSTORE_PSA_ALG_CBC_MAC   ((KeyStore_PSA_Algorithm)PSA_ALG_CBC_MAC)

The CBC-MAC construction over a block cipher

Warning
CBC-MAC is insecure in many cases. A more secure mode, such as KEYSTORE_PSA_ALG_CMAC, is recommended.

§ KEYSTORE_PSA_ALG_CMAC

#define KEYSTORE_PSA_ALG_CMAC   ((KeyStore_PSA_Algorithm)PSA_ALG_CMAC)

The CMAC construction over a block cipher

§ KEYSTORE_PSA_ALG_CTR

#define KEYSTORE_PSA_ALG_CTR   ((KeyStore_PSA_Algorithm)PSA_ALG_CTR)

The CTR stream cipher mode.

CTR is a stream cipher which is built from a block cipher. The underlying block cipher is determined by the key type. For example, to use AES-128-CTR, use this algorithm with a key of type KEYSTORE_PSA_KEY_TYPE_AES and a length of 128 bits (16 bytes).

§ KEYSTORE_PSA_ALG_ECB_NO_PADDING

#define KEYSTORE_PSA_ALG_ECB_NO_PADDING   ((KeyStore_PSA_Algorithm)PSA_ALG_ECB_NO_PADDING)

The Electronic Code Book (ECB) mode of a block cipher, with no padding.

Warning
ECB mode does not protect the confidentiality of the encrypted data except in extremely narrow circumstances. It is recommended that applications only use ECB if they need to construct an operating mode that the implementation does not provide. Implementations are encouraged to provide the modes that applications need in preference to supporting direct access to ECB.

The underlying block cipher is determined by the key type.

This symmetric cipher mode can only be used with messages whose lengths are a multiple of the block size of the chosen block cipher.

§ KEYSTORE_PSA_ALG_CBC_NO_PADDING

#define KEYSTORE_PSA_ALG_CBC_NO_PADDING   ((KeyStore_PSA_Algorithm)PSA_ALG_CBC_NO_PADDING)

The CBC block cipher chaining mode, with no padding.

The underlying block cipher is determined by the key type.

This symmetric cipher mode can only be used with messages whose lengths are whole number of blocks for the chosen block cipher.

§ KEYSTORE_PSA_ALG_CCM

#define KEYSTORE_PSA_ALG_CCM   ((KeyStore_PSA_Algorithm)PSA_ALG_CCM)

The CCM authenticated encryption algorithm.

The underlying block cipher is determined by the key type.

§ KEYSTORE_PSA_ALG_GCM

#define KEYSTORE_PSA_ALG_GCM   ((KeyStore_PSA_Algorithm)PSA_ALG_GCM)

The GCM authenticated encryption algorithm.

The underlying block cipher is determined by the key type.

§ KEYSTORE_PSA_ALG_CHACHA20_POLY1305

#define KEYSTORE_PSA_ALG_CHACHA20_POLY1305   ((KeyStore_PSA_Algorithm)PSA_ALG_CHACHA20_POLY1305)

The Chacha20-Poly1305 AEAD algorithm.

The ChaCha20_Poly1305 construction is defined in RFC 7539.

Implementations must support 12-byte nonces, may support 8-byte nonces, and should reject other sizes.

Implementations must support 16-byte tags and should reject other sizes.

§ KEYSTORE_PSA_ALG_ECDH

#define KEYSTORE_PSA_ALG_ECDH   ((KeyStore_PSA_Algorithm)PSA_ALG_ECDH)

The elliptic curve Diffie-Hellman (ECDH) key agreement algorithm.

The shared secret produced by key agreement is the x-coordinate of the shared secret point. It is always ceiling(m / 8) bytes long where m is the bit size associated with the curve, i.e. the bit size of the order of the curve's coordinate field. When m is not a multiple of 8, the byte containing the most significant bit of the shared secret is padded with zero bits. The byte order is either little-endian or big-endian depending on the curve type.

  • For Montgomery curves (curve types PSA_ECC_FAMILY_CURVEXXX), the shared secret is the x-coordinate of d_A Q_B = d_B Q_A in little-endian byte order. The bit size is 448 for Curve448 and 255 for Curve25519.
  • For Weierstrass curves over prime fields (curve types PSA_ECC_FAMILY_SECPXXX and PSA_ECC_FAMILY_BRAINPOOL_PXXX), the shared secret is the x-coordinate of d_A Q_B = d_B Q_A in big-endian byte order. The bit size is m = ceiling(log_2(p)) for the field F_p.
  • For Weierstrass curves over binary fields (curve types PSA_ECC_FAMILY_SECTXXX), the shared secret is the x-coordinate of d_A Q_B = d_B Q_A in big-endian byte order. The bit size is m for the field F_{2^m}.

§ KEYSTORE_PSA_ALG_ECDSA

#define KEYSTORE_PSA_ALG_ECDSA   ((KeyStore_PSA_Algorithm)PSA_ALG_ECDSA_ANY)

ECDSA signature without hashing.

This is the same signature scheme without specifying a hash algorithm. This algorithm may only be used to sign or verify a sequence of bytes that should be an pre-calculated hash.

§ KEYSTORE_PSA_ALG_PAKE

#define KEYSTORE_PSA_ALG_PAKE   ((KeyStore_PSA_Algorithm)PSA_ALG_JPAKE)

The Password-authenticated key exchange by juggling (J-PAKE) algorithm.

§ KEYSTORE_PSA_ALG_PURE_EDDSA

#define KEYSTORE_PSA_ALG_PURE_EDDSA   ((KeyStore_PSA_Algorithm)PSA_ALG_PURE_EDDSA)

Edwards-curve digital signature algorithm without prehashing (PureEdDSA), using standard parameters.

PureEdDSA requires an elliptic curve key on a twisted Edwards curve. In this specification, the following curves are supported:

  • PSA_ECC_FAMILY_TWISTED_EDWARDS, 255-bit: Ed25519 as specified in RFC 8032. The curve is Edwards25519. The hash function used internally is SHA-512.

This algorithm can be used with KEYSTORE_PSA_KEY_USAGE_SIGN_MESSAGE and KEYSTORE_PSA_KEY_USAGE_VERIFY_MESSAGE. Since there is no prehashing, it cannot be used with KEYSTORE_PSA_KEY_USAGE_SIGN_HASH and KEYSTORE_PSA_KEY_USAGE_VERIFY_HASH.

§ KEYSTORE_PSA_ECC_CURVE_SECT163K1

#define KEYSTORE_PSA_ECC_CURVE_SECT163K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)

§ KEYSTORE_PSA_ECC_CURVE_SECT163R1

#define KEYSTORE_PSA_ECC_CURVE_SECT163R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECT163R2

#define KEYSTORE_PSA_ECC_CURVE_SECT163R2   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R2)

§ KEYSTORE_PSA_ECC_CURVE_SECT193R1

#define KEYSTORE_PSA_ECC_CURVE_SECT193R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECT193R2

#define KEYSTORE_PSA_ECC_CURVE_SECT193R2   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R2)

§ KEYSTORE_PSA_ECC_CURVE_SECT233K1

#define KEYSTORE_PSA_ECC_CURVE_SECT233K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)

§ KEYSTORE_PSA_ECC_CURVE_SECT233R1

#define KEYSTORE_PSA_ECC_CURVE_SECT233R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECT239K1

#define KEYSTORE_PSA_ECC_CURVE_SECT239K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)

§ KEYSTORE_PSA_ECC_CURVE_SECT283K1

#define KEYSTORE_PSA_ECC_CURVE_SECT283K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)

§ KEYSTORE_PSA_ECC_CURVE_SECT283R1

#define KEYSTORE_PSA_ECC_CURVE_SECT283R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECT409K1

#define KEYSTORE_PSA_ECC_CURVE_SECT409K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)

§ KEYSTORE_PSA_ECC_CURVE_SECT409R1

#define KEYSTORE_PSA_ECC_CURVE_SECT409R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECT571K1

#define KEYSTORE_PSA_ECC_CURVE_SECT571K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)

§ KEYSTORE_PSA_ECC_CURVE_SECT571R1

#define KEYSTORE_PSA_ECC_CURVE_SECT571R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECP160K1

#define KEYSTORE_PSA_ECC_CURVE_SECP160K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)

§ KEYSTORE_PSA_ECC_CURVE_SECP160R1

#define KEYSTORE_PSA_ECC_CURVE_SECP160R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECP160R2

#define KEYSTORE_PSA_ECC_CURVE_SECP160R2   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R2)

§ KEYSTORE_PSA_ECC_CURVE_SECP192K1

#define KEYSTORE_PSA_ECC_CURVE_SECP192K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)

§ KEYSTORE_PSA_ECC_CURVE_SECP192R1

#define KEYSTORE_PSA_ECC_CURVE_SECP192R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECP224K1

#define KEYSTORE_PSA_ECC_CURVE_SECP224K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)

§ KEYSTORE_PSA_ECC_CURVE_SECP224R1

#define KEYSTORE_PSA_ECC_CURVE_SECP224R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECP256K1

#define KEYSTORE_PSA_ECC_CURVE_SECP256K1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_K1)

§ KEYSTORE_PSA_ECC_CURVE_SECP256R1

#define KEYSTORE_PSA_ECC_CURVE_SECP256R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECP384R1

#define KEYSTORE_PSA_ECC_CURVE_SECP384R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_PSA_ECC_CURVE_SECP521R1

#define KEYSTORE_PSA_ECC_CURVE_SECP521R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_SECP_R1)

§ KEYSTORE_ECC_CURVE_BRAINPOOL_P256R1

#define KEYSTORE_ECC_CURVE_BRAINPOOL_P256R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_BRAINPOOL_P_R1)

§ KEYSTORE_ECC_CURVE_BRAINPOOL_P384R1

#define KEYSTORE_ECC_CURVE_BRAINPOOL_P384R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_BRAINPOOL_P_R1)

§ KEYSTORE_ECC_CURVE_BRAINPOOL_P512R1

#define KEYSTORE_ECC_CURVE_BRAINPOOL_P512R1   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_BRAINPOOL_P_R1)

§ KEYSTORE_PSA_ECC_CURVE_ED25519

#define KEYSTORE_PSA_ECC_CURVE_ED25519   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_TWISTED_EDWARDS)

Ed25519

PureEdDSA requires an elliptic curve key on a twisted Edwards curve. In this specification, the following curves are supported:

  • PSA_ECC_FAMILY_TWISTED_EDWARDS, 255-bit: Ed25519 as specified in RFC 8032. The curve is Edwards25519. The hash function used internally is SHA-512. The algorithm KEYSTORE_PSA_ALG_PURE_EDDSA performs ed25519 when used with this curve.

§ KEYSTORE_PSA_ECC_CURVE_CURVE25519

#define KEYSTORE_PSA_ECC_CURVE_CURVE25519   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_MONTGOMERY)

Curve25519

This is the curve defined in Bernstein et al., Curve25519: new Diffie-Hellman speed records, LNCS 3958, 2006. The algorithm KEYSTORE_PSA_ALG_ECDH performs X25519 when used with this curve.

§ KEYSTORE_PSA_ECC_CURVE_CURVE448

#define KEYSTORE_PSA_ECC_CURVE_CURVE448   ((KeyStore_PSA_KeyType)PSA_ECC_FAMILY_MONTGOMERY)

Curve448

This is the curve defined in Hamburg, Ed448-Goldilocks, a new elliptic curve, NIST ECC Workshop, 2015. The algorithm KEYSTORE_PSA_ALG_ECDH performs X448 when used with this curve.

§ KEYSTORE_PSA_ECC_CURVE_VENDOR_MIN

#define KEYSTORE_PSA_ECC_CURVE_VENDOR_MIN   ((KeyStore_PSA_KeyType)PSA_ECC_CURVE_VENDOR_MIN)

Minimum value for a vendor-defined ECC curve identifier

The range for vendor-defined curve identifiers is a subset of the IANA registry private use range, 0xfe00 - 0xfeff.

§ KEYSTORE_PSA_ECC_CURVE_VENDOR_MAX

#define KEYSTORE_PSA_ECC_CURVE_VENDOR_MAX   ((KeyStore_PSA_KeyType)PSA_ECC_CURVE_VENDOR_MAX)

Maximum value for a vendor-defined ECC curve identifier

The range for vendor-defined curve identifiers is a subset of the IANA registry private use range, 0xfe00 - 0xfeff.

§ KEYSTORE_PSA_MIN_VOLATILE_KEY_ID

#define KEYSTORE_PSA_MIN_VOLATILE_KEY_ID   PSA_KEY_ID_VOLATILE_MIN

Volatile Key Limit [KEYSTORE_PSA_MIN_VOLATILE_KEY_ID, KEYSTORE_PSA_MAX_VOLATILE_KEY_ID]

Upper limit for volatile key ID, KEYSTORE_PSA_MIN_VOLATILE_KEY_ID, is KEYSTORE_PSA_KEY_ID_VENDOR_MAX. Lower limit for volatile key ID, KEYSTORE_PSA_MIN_VOLATILE_KEY_ID, is the last MBEDTLS_PSA_KEY_SLOT_COUNT identifiers of provided by implementation reserved for vendors.

§ KEYSTORE_PSA_MAX_VOLATILE_KEY_ID

#define KEYSTORE_PSA_MAX_VOLATILE_KEY_ID   PSA_KEY_ID_VOLATILE_MAX

§ MEMBER_SIZE

#define MEMBER_SIZE (   type,
  member 
)    sizeof(((type *)0)->member)

§ KEYSTORE_PSA_PREPROVISIONED_AREA_ADDR

#define KEYSTORE_PSA_PREPROVISIONED_AREA_ADDR   0x0000

Starting address of Pre-provisioned keys.

The Immutable platform Root of Trust stores the pre-provisioned key's programmed at production. SKS implementation will read this address to obtain the KeyStore_PSA_KeyFileId and other relevant meta data of all the pre-provisioned keys stored at this address

§ KEYSTORE_PSA_PREPROVISIONED_AREA_SIZE

#define KEYSTORE_PSA_PREPROVISIONED_AREA_SIZE   (0x700) /* 1792 B */

Area size for pre-provisioned keys, 2KB - 256B (reserved for attestation data)

§ KEYSTORE_PSA_PREPROVISIONED_KEYS_EMPTY

#define KEYSTORE_PSA_PREPROVISIONED_KEYS_EMPTY   0xFFFF

Macro to indicate empty pre-provisioned key memory.

§ KEYSTORE_PSA_PRE_PROVISIONED_KEY_MAGIC_HEADER

#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_MAGIC_HEADER   "HUK\0KEY"

Pre-provisioned key storage magic header.

§ KEYSTORE_PSA_PRE_PROVISIONED_KEYS_END

#define KEYSTORE_PSA_PRE_PROVISIONED_KEYS_END   0

§ KEYSTORE_PSA_PRE_PROVISIONED_KEY_MAGIC_HEADER_LENGTH

#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_MAGIC_HEADER_LENGTH   (sizeof(KEYSTORE_PSA_PRE_PROVISIONED_KEY_MAGIC_HEADER))

§ KEYSTORE_PSA_PRE_PROVISIONED_KEYS_END_LENGTH

#define KEYSTORE_PSA_PRE_PROVISIONED_KEYS_END_LENGTH   (sizeof(KEYSTORE_PSA_PRE_PROVISIONED_KEYS_END))

§ KEYSTORE_PSA_MAX_PREPROVISIONED_KEYS

#define KEYSTORE_PSA_MAX_PREPROVISIONED_KEYS   0x10

§ KEYSTORE_PSA_PRE_PROVISIONED_KEY_VALID_LIFETIME

#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_VALID_LIFETIME   0xAAAA

Pre-provisioned key Lifetime.

§ KEYSTORE_PSA_PRE_PROVISIONED_KEY_INVALID_LIFETIME

#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_INVALID_LIFETIME   0x8888

§ KEYSTORE_PSA_PRE_PROVISIONED_KEY_ID_MAX

#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_ID_MAX   MBEDTLS_PSA_KEY_ID_BUILTIN_MAX

Admissible key ID range for Pre-provisioned keys.

0x7fff0000 - 0x7fffefff is reserved to store pre-provisioned keys.

§ KEYSTORE_PSA_PRE_PROVISIONED_KEY_ID_MIN

#define KEYSTORE_PSA_PRE_PROVISIONED_KEY_ID_MIN   MBEDTLS_PSA_KEY_ID_BUILTIN_MIN

Typedef Documentation

§ KeyStore_PSA_KeyUsage

typedef psa_key_usage_t KeyStore_PSA_KeyUsage

Encoding of permitted usage on a key.

§ KeyStore_PSA_KeyLifetime

typedef psa_key_lifetime_t KeyStore_PSA_KeyLifetime

Encoding of key lifetimes.

The lifetime of a key indicates where it is stored and what system actions may create and destroy it.

Lifetime values have the following structure:

Volatile keys are automatically destroyed when the application instance terminates or on a power reset of the device. Persistent keys are preserved until the application explicitly destroys them or until an integration-specific device management event occurs (for example, a factory reset).

Persistent keys have a key identifier of type KeyStore_PSA_KeyFileId. This identifier remains valid throughout the lifetime of the key, even if the application instance that created the key terminates.

The default lifetime of a key is KEYSTORE_PSA_KEY_LIFETIME_VOLATILE. The lifetime KEYSTORE_PSA_KEY_LIFETIME_PERSISTENT is supported if persistent storage is available. Other lifetime values may be supported depending on the library configuration.

Values of this type are generally constructed by macros called KEYSTORE_PSA_KEY_LIFETIME_xxx.

Note
Values of this type are encoded in the persistent key store. Any changes to existing values will require bumping the storage format version and providing a translation when reading the old format.

§ KeyStore_PSA_KeyPersistence

typedef psa_key_persistence_t KeyStore_PSA_KeyPersistence

Encoding of key persistence levels.

What distinguishes different persistence levels is what device management events may cause keys to be destroyed. Volatile keys are destroyed by a power reset. Persistent keys may be destroyed by events such as a transfer of ownership or a factory reset. What management events actually affect persistent keys at different levels is outside the scope of the PSA Cryptography specification.

The PSA Cryptography specification defines the following values of persistence levels:

  • 0 = KEYSTORE_PSA_KEY_PERSISTENCE_VOLATILE: volatile key. A volatile key is automatically destroyed by the implementation when the application instance terminates. In particular, a volatile key is automatically destroyed on a power reset of the device.
  • 1 = KEYSTORE_PSA_KEY_PERSISTENCE_DEFAULT: persistent key with a default lifetime.
  • 2-254: currently not supported by Mbed TLS.
  • 255 = KEYSTORE_PSA_KEY_PERSISTENCE_READ_ONLY: read-only or write-once key. A key with this persistence level cannot be destroyed. Mbed TLS does not currently offer a way to create such keys, but integrations of Mbed TLS can use it for built-in keys that the application cannot modify (for example, a hardware unique key (HUK)).
Note
Key persistence levels are 8-bit values. Key management interfaces operate on lifetimes (type KeyStore_PSA_KeyLifetime) which encode the persistence as the lower 8 bits of a 32-bit value.
Values of this type are encoded in the persistent key store. Any changes to existing values will require bumping the storage format version and providing a translation when reading the old format.

§ KeyStore_PSA_KeyLocation

typedef psa_key_location_t KeyStore_PSA_KeyLocation

Encoding of key location indicators.

If an application can make calls to external cryptoprocessors such as secure elements, the location of a key indicates which secure element performs the operations on the key. Depending on the design of the secure element, the key material may be stored either in the secure element, or in wrapped (encrypted) form alongside the key metadata in the primary local storage.

The PSA Cryptography API specification defines the following values of location indicators:

  • 0: primary local storage. This location is always available. The primary local storage is typically the same storage area that contains the key metadata.
  • 1: primary secure element. Integrations of Mbed TLS should support this value if there is a secure element attached to the operating environment. As a guideline, secure elements may provide higher resistance against side channel and physical attacks than the primary local storage, but may have restrictions on supported key types, sizes, policies and operations and may have different performance characteristics.
  • 2-0x7fffff: other locations defined by a PSA specification. The PSA Cryptography API does not currently assign any meaning to these locations, but future versions of that specification or other PSA specifications may do so.
  • 0x800000-0xffffff: vendor-defined locations. No PSA specification will assign a meaning to locations in this range.
Note
Key location indicators are 24-bit values. Key management interfaces operate on lifetimes (type KeyStore_PSA_KeyLifetime) which encode the location as the upper 24 bits of a 32-bit value.
Values of this type are encoded in the persistent key store. Any changes to existing values will require bumping the storage format version and providing a translation when reading the old format.

§ KeyStore_PSA_KeyType

typedef psa_key_type_t KeyStore_PSA_KeyType

Encoding of a key type.

§ KeyStore_PSA_Algorithm

typedef psa_algorithm_t KeyStore_PSA_Algorithm

Encoding of a cryptographic algorithm.

For algorithms that can be applied to multiple key types, this type does not encode the key type. For example, for symmetric ciphers based on a block cipher, KeyStore_PSA_Algorithm encodes the block cipher mode and the padding mode while the block cipher itself is encoded via KeyStore_PSA_KeyType.

Function Documentation

§ KeyStore_PSA_setKeyId()

void KeyStore_PSA_setKeyId ( KeyStore_PSA_KeyAttributes attributes,
KeyStore_PSA_KeyFileId  key 
)

Declare a key as persistent and set its key identifier.

If the attribute structure currently declares the key as volatile (which is the default content of an attribute structure), this function sets the lifetime attribute to KEYSTORE_PSA_KEY_LIFETIME_PERSISTENT.

This function does not access storage, it merely stores the given value in the structure. The persistent key will be written to storage when the attribute structure is passed to a key creation function such as KeyStore_PSA_import_key(), KeyStore_PSA_generate_key(), KeyStore_PSA_key_derivation_output_key() or KeyStore_PSA_copy_key().

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
keyThe persistent identifier for the key.

§ KeyStore_PSA_setKeyLifetime()

void KeyStore_PSA_setKeyLifetime ( KeyStore_PSA_KeyAttributes attributes,
KeyStore_PSA_KeyLifetime  lifetime 
)

Set the location of a persistent key.

To make a key persistent, you must give it a persistent key identifier with KeyStore_PSA_setKeyId(). By default, a key that has a persistent identifier is stored in the default storage area identifier by KEYSTORE_PSA_KEY_LIFETIME_PERSISTENT. Call this function to choose a storage area, or to explicitly declare the key as volatile.

This function does not access storage, it merely stores the given value in the structure. The persistent key will be written to storage when the attribute structure is passed to a key creation function such as KeyStore_PSA_import_key(), KeyStore_PSA_generate_key(), KeyStore_PSA_key_derivation_output_key() or KeyStore_PSA_copy_key().

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
lifetimeThe lifetime for the key. If this is KEYSTORE_PSA_KEY_LIFETIME_VOLATILE, the key will be volatile, and the key identifier attribute is reset to 0.

§ KeyStore_PSA_getKeyId()

KeyStore_PSA_KeyFileId KeyStore_PSA_getKeyId ( KeyStore_PSA_KeyAttributes attributes)

Retrieve the key identifier from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The persistent identifier stored in the attribute structure. This value is unspecified if the attribute structure declares the key as volatile.

§ KeyStore_PSA_getKeyLifetime()

KeyStore_PSA_KeyLifetime KeyStore_PSA_getKeyLifetime ( KeyStore_PSA_KeyAttributes attributes)

Retrieve the lifetime from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The lifetime value stored in the attribute structure.

§ KeyStore_PSA_setKeyUsageFlags()

void KeyStore_PSA_setKeyUsageFlags ( KeyStore_PSA_KeyAttributes attributes,
KeyStore_PSA_KeyUsage  usageFlags 
)

Declare usage flags for a key.

Usage flags are part of a key's usage policy. They encode what kind of operations are permitted on the key. For more details, refer to the documentation of the type KeyStore_PSA_KeyUsage.

This function overwrites any usage flags previously set in attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
usageFlagsThe usage flags to write.

§ KeyStore_PSA_getKeyUsageFlags()

KeyStore_PSA_KeyUsage KeyStore_PSA_getKeyUsageFlags ( KeyStore_PSA_KeyAttributes attributes)

Retrieve the usage flags from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The usage flags stored in the attribute structure.

§ KeyStore_PSA_setKeyAlgorithm()

void KeyStore_PSA_setKeyAlgorithm ( KeyStore_PSA_KeyAttributes attributes,
KeyStore_PSA_Algorithm  alg 
)

Declare the permitted algorithm policy for a key.

The permitted algorithm policy of a key encodes which algorithm or algorithms are permitted to be used with this key. The following algorithm policies are supported:

  • 0 does not allow any cryptographic operation with the key. The key may be used for non-cryptographic actions such as exporting (if permitted by the usage flags).
  • An algorithm value permits this particular algorithm.

This function overwrites any algorithm policy previously set in attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
algThe permitted algorithm policy to write.

§ KeyStore_PSA_getKeyAlgorithm()

KeyStore_PSA_Algorithm KeyStore_PSA_getKeyAlgorithm ( KeyStore_PSA_KeyAttributes attributes)

Retrieve the algorithm policy from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The algorithm stored in the attribute structure.

§ KeyStore_PSA_setKeyType()

void KeyStore_PSA_setKeyType ( KeyStore_PSA_KeyAttributes attributes,
KeyStore_PSA_KeyType  type 
)

Declare the type of a key.

This function overwrites any key type previously set in attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
typeThe key type to write. If this is 0, the key type in attributes becomes unspecified.

§ KeyStore_PSA_setKeyBits()

void KeyStore_PSA_setKeyBits ( KeyStore_PSA_KeyAttributes attributes,
size_t  bits 
)

Declare the size of a key.

This function overwrites any key size previously set in attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
bitsThe key size in bits. If this is 0, the key size in attributes becomes unspecified. Keys of size 0 are not supported.

§ KeyStore_PSA_getKeyType()

KeyStore_PSA_KeyType KeyStore_PSA_getKeyType ( KeyStore_PSA_KeyAttributes attributes)

Retrieve the key type from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The key type stored in the attribute structure.

§ KeyStore_PSA_getKeyBits()

size_t KeyStore_PSA_getKeyBits ( KeyStore_PSA_KeyAttributes attributes)

Retrieve the key size from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The key size stored in the attribute structure, in bits.

§ KeyStore_PSA_resetKeyAttributes()

void KeyStore_PSA_resetKeyAttributes ( KeyStore_PSA_KeyAttributes attributes)

Reset a key attribute structure to a freshly initialized state.

You must initialize the attribute structure as described in the documentation of the type KeyStore_PSA_KeyAttributes before calling this function. Once the structure has been initialized, you may call this function at any time.

This function frees any auxiliary resources that the structure may contain.

Parameters
[in,out]attributesThe attribute structure to reset.

§ KeyStore_PSA_exportPublicKey()

int_fast16_t KeyStore_PSA_exportPublicKey ( KeyStore_PSA_KeyFileId  key,
uint8_t *  data,
size_t  dataSize,
size_t *  dataLength 
)

Export a public key or the public part of a key pair in binary format.

The output of this function can be passed to KeyStore_PSA_importKey() to create an object that is equivalent to the public key.

This specification supports a single format for each key type. Implementations may support other formats as long as the standard format is supported. Implementations that support other formats should ensure that the formats are clearly unambiguous so as to minimize the risk that an invalid input is accidentally interpreted according to a different format.

  • For elliptic curve public keys, the format for:
    • Montgomery curves (curve types PSA_ECC_CURVE_CURVEXXX), is
      • x_P as a ceiling(m/8)-byte string, little-endian;
    • Weierstrass curves (curve types PSA_ECC_CURVE_SECTXXX, PSA_ECC_CURVE_SECPXXX and PSA_ECC_CURVE_BRAINPOOL_PXXX), is the uncompressed representation defined by SEC1 §2.3.3 as the content of an ECPoint. Let m be the bit size associated with the curve, i.e. the bit size of q for a curve over F_q. The representation consists of:
      • The byte 0x04;
      • x_P as a ceiling(m/8)-byte string, big-endian;
      • y_P as a ceiling(m/8)-byte string, big-endian.
  • For Diffie-Hellman key exchange public keys, the format is the representation of the public key y = g^x mod p as a big-endian byte string. The length of the byte string is the length of the base prime p in bytes.

Exporting a public key object or the public part of a key pair is always permitted, regardless of the key's usage flags.

Parameters
[in]keyKey file ID of the key to export.
[out]dataBuffer where the key data is to be written.
[in]dataSizeSize of the data buffer in bytes.
[out]dataLengthOn success, the number of bytes that make up the key data.
Return values
KEYSTORE_PSA_STATUS_SUCCESS
KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLEIf the KeyStore lock cannot be acquired, the KeyStore module is in use elsewhere.
KEYSTORE_PSA_STATUS_INVALID_KEY_ID
KEYSTORE_PSA_STATUS_INVALID_ARGUMENTThe key is neither a public key nor a key pair.
KEYSTORE_PSA_STATUS_NOT_SUPPORTED
KEYSTORE_PSA_STATUS_BUFFER_TOO_SMALLThe size of the data buffer is too small.
KEYSTORE_PSA_STATUS_COMMUNICATION_FAILURE
KEYSTORE_PSA_STATUS_HARDWARE_FAILURE
KEYSTORE_PSA_STATUS_CORRUPTION_DETECTED
KEYSTORE_PSA_STATUS_STORAGE_FAILURE
KEYSTORE_PSA_STATUS_INSUFFICIENT_MEMORY
KEYSTORE_PSA_STATUS_BAD_STATEThe library has not been previously initialized by KeyStore_PSA_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ KeyStore_PSA_exportKey()

int_fast16_t KeyStore_PSA_exportKey ( KeyStore_PSA_KeyFileId  key,
uint8_t *  data,
size_t  dataSize,
size_t *  dataLength 
)

Export a key in binary format.

The key must designated as exportable. The output of this function can be passed to KeyStore_PSA_importKey() to create an equivalent object.

If the implementation of KeyStore_PSA_importKey() supports other formats beyond the format specified here, the output from KeyStore_PSA_exportKey() must use the representation specified here, not the original representation.

For standard key types, the output format is as follows:

  • For symmetric keys (including MAC keys), the format is the raw bytes of the key.
  • For elliptic curve key pairs, the format is a representation of the private value as a ceiling(m/8)-byte string where m is the bit size associated with the curve, i.e. the bit size of the order of the curve's coordinate field. This byte string is in little-endian order for Montgomery curves (curve types PSA_ECC_CURVE_CURVEXXX), and in big-endian order for Weierstrass curves (curve types PSA_ECC_CURVE_SECTXXX, PSA_ECC_CURVE_SECPXXX and PSA_ECC_CURVE_BRAINPOOL_PXXX). This is the content of the privateKey field of the ECPrivateKey format defined by RFC 5915.
  • For Diffie-Hellman key exchange key pairs, the format is the representation of the private key x as a big-endian byte string. The length of the byte string is the private key size in bytes (leading zeroes are not stripped).
  • For public keys, the format is the same as for KeyStore_PSA_exportPublicKey().

This function can also be used to export other sensitive data, such as certificates using its corresponding key file ID.

The policy on the key must have the usage flag KEYSTORE_PSA_KEY_USAGE_EXPORT set.

Parameters
[in]keyKey file ID of the key to export.
[out]dataBuffer where the key data is to be written.
[in]dataSizeSize of the data buffer in bytes.
[out]dataLengthOn success, the number of bytes that make up the key data.
Return values
KEYSTORE_PSA_STATUS_SUCCESS
KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLEIf the KeyStore lock cannot be acquired, the KeyStore module is in use elsewhere.
KEYSTORE_PSA_STATUS_INVALID_KEY_IDThe key identifier does not exist.
KEYSTORE_PSA_STATUS_NOT_PERMITTEDThe key does not have the KEYSTORE_PSA_KEY_USAGE_EXPORT flag.
KEYSTORE_PSA_STATUS_NOT_SUPPORTED
KEYSTORE_PSA_STATUS_BUFFER_TOO_SMALLThe size of the data buffer is too small.
KEYSTORE_PSA_STATUS_STORAGE_FAILURE
KEYSTORE_PSA_STATUS_INSUFFICIENT_MEMORY
KEYSTORE_PSA_STATUS_BAD_STATEThe library has not been previously initialized by KeyStore_PSA_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ KeyStore_PSA_importKey()

int_fast16_t KeyStore_PSA_importKey ( KeyStore_PSA_KeyAttributes attributes,
uint8_t *  data,
size_t  dataLength,
KeyStore_PSA_KeyFileId key 
)

Import a key in binary format.

This function supports any output from KeyStore_PSA_exportKey(). Refer to the documentation of KeyStore_PSA_exportPublicKey() for the format of public keys and to the documentation of KeyStore_PSA_exportKey() for the format for other key types.

The dataLength determines the key size. The attributes may optionally specify a key size; in this case it must match the dataLength. A key size of 0 in attributes indicates that the key size is solely determined by the key data.

Implementations must reject an attempt to import a key of size 0.

This specification supports a single format for each key type. Implementations may support other formats as long as the standard format is supported. Implementations that support other formats should ensure that the formats are clearly unambiguous so as to minimize the risk that an invalid input is accidentally interpreted according to a different format.

This function can also be used to store other sensitive data, such as certificate using key type KEYSTORE_PSA_KEY_TYPE_RAW_DATA.

Parameters
[in]attributesThe attributes for the new key. The key size is always determined from the data buffer. If the key size in attributes is nonzero, it must be equal to the size from data.
[in]dataBuffer containing the key data. The content of this buffer is interpreted according to the type declared in attributes. All implementations must support at least the format described in the documentation of KeyStore_PSA_exportKey() or KeyStore_PSA_exportPublicKey() for the chosen type. Implementations may allow other formats, but should be conservative: implementations should err on the side of rejecting content if it may be erroneous (e.g. wrong type or truncated data).
[in]dataLengthSize of the data buffer in bytes.
[out]keyOn success, the key file ID of the newly created key. 0 on failure.
Return values
KEYSTORE_PSA_STATUS_SUCCESSSuccess. If the key is persistent, the key material and the key's metadata have been saved to persistent storage.
KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLEIf the KeyStore lock cannot be acquired, the KeyStore module is in use elsewhere.
KEYSTORE_PSA_STATUS_ALREADY_EXISTSThis is an attempt to create a key, and there is already a key with the given key file identifier.
KEYSTORE_PSA_STATUS_NOT_SUPPORTEDThe key type or key size is not supported, either by the implementation in general or in this particular persistent location.
KEYSTORE_PSA_STATUS_INVALID_ARGUMENTThe key attributes, as a whole, are invalid.
KEYSTORE_PSA_STATUS_INVALID_ARGUMENTThe key data is not correctly formatted.
KEYSTORE_PSA_STATUS_INVALID_ARGUMENTThe size in attributes is nonzero and does not match the size of the key data.
KEYSTORE_PSA_STATUS_INSUFFICIENT_MEMORY
KEYSTORE_PSA_STATUS_INSUFFICIENT_STORAGE
KEYSTORE_PSA_STATUS_COMMUNICATION_FAILURE
KEYSTORE_PSA_STATUS_STORAGE_FAILURE
KEYSTORE_PSA_STATUS_HARDWARE_FAILURE
KEYSTORE_PSA_STATUS_CORRUPTION_DETECTED
KEYSTORE_PSA_STATUS_BAD_STATEThe library has not been previously initialized by KeyStore_PSA_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ KeyStore_PSA_getKeyAttributes()

int_fast16_t KeyStore_PSA_getKeyAttributes ( KeyStore_PSA_KeyFileId  key,
KeyStore_PSA_KeyAttributes attributes 
)

Retrieve the attributes of a key.

This function first resets the attribute structure as with KeyStore_PSA_resetKeyAttributes(). It then copies the attributes of the given key into the given attribute structure.

Note
This function may allocate memory or other resources. Once you have called this function on an attribute structure, you must call KeyStore_PSA_resetKeyAttributes() to free these resources.
Parameters
[in]keyIdentifier of the key to query.
[in,out]attributesOn success, the attributes of the key. On failure, equivalent to a freshly-initialized structure.
Return values
KEYSTORE_PSA_STATUS_SUCCESS
KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLEIf the KeyStore lock cannot be acquired, the KeyStore module is in use elsewhere.
KEYSTORE_PSA_STATUS_INVALID_KEY_ID
KEYSTORE_PSA_STATUS_INSUFFICIENT_MEMORY
KEYSTORE_PSA_STATUS_COMMUNICATION_FAILURE
KEYSTORE_PSA_STATUS_CORRUPTION_DETECTED
KEYSTORE_PSA_STATUS_STORAGE_FAILURE
KEYSTORE_PSA_STATUS_BAD_STATEThe library has not been previously initialized by KeyStore_PSA_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ KeyStore_PSA_purgeKey()

int_fast16_t KeyStore_PSA_purgeKey ( KeyStore_PSA_KeyFileId  key)

Remove non-essential copies of key material from memory.

An implementation is permitted to make additional copies of key material for keys that have been created with the cache policy, an implementation is permitted to make additional copies of the key material that are not in storage and not for the purpose of ongoing operations. This function will remove these extra copies of the key material from memory.

This function is not required to remove key material from memory in any of the following situations:

  • The key is currently in use in a cryptographic operation.
  • The key is volatile
Parameters
[in]keyKey handle to close. . If this is 0, do nothing and return KEYSTORE_PSA_STATUS_SUCCESS.
Return values
KEYSTORE_PSA_STATUS_SUCCESSHandle was valid and the key material that it referred to has been closed. Alternatively, Handle is 0.
KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLEIf the KeyStore lock cannot be acquired, the KeyStore module is in use elsewhere.
KEYSTORE_PSA_STATUS_INVALID_KEY_IDhandle is not a valid handle nor 0.
KEYSTORE_PSA_STATUS_COMMUNICATION_FAILUREThere was an failure in communication with the cryptoprocessor. The key material may still be present in the cryptoprocessor.
KEYSTORE_PSA_STATUS_STORAGE_FAILUREThe storage is corrupted. Implementations shall make a best effort to erase key material even in this stage, however applications should be aware that it may be impossible to guarantee that the key material is not recoverable in such cases.
KEYSTORE_PSA_STATUS_CORRUPTION_DETECTEDAn unexpected condition which is not a storage corruption or a communication failure occurred. The cryptoprocessor may have been compromised.
KEYSTORE_PSA_STATUS_BAD_STATEThe library has not been previously initialized by KeyStore_PSA_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ KeyStore_PSA_destroyKey()

int_fast16_t KeyStore_PSA_destroyKey ( KeyStore_PSA_KeyFileId  key)

Destroy a key.

This function destroys a key from both volatile memory and, if applicable, non-volatile storage. Implementations shall make a best effort to ensure that that the key material cannot be recovered.

This function also erases any metadata such as policies and frees resources associated with the key.

Destroying the key makes the ID invalid, and the key ID must not be used again by the application.

If a key is currently in use in a multipart operation, then destroying the key will cause the multipart operation to fail.

After a volatile key is destroyed, it is recommended that the implementation does not immediately reuse the same key ID value for a different key. This reduces the risk of an attack that is able to exploit a key identifier reuse vulnerability within an application.

This function can also be used to destroy other sensitive data, such as certificates using its corresponding key file ID.

Parameters
[in]keyKey file ID of the key to erase. If key ID portion is 0, do nothing and return KEYSTORE_PSA_STATUS_SUCCESS.
Return values
KEYSTORE_PSA_STATUS_SUCCESSID was a valid ID and the key material that it referred to has been erased. Alternatively, ID is 0.
KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLEIf the KeyStore lock cannot be acquired, the KeyStore module is in use elsewhere.
KEYSTORE_PSA_STATUS_NOT_PERMITTEDThe key cannot be erased because it is read-only, either due to a policy or due to physical restrictions.
KEYSTORE_PSA_STATUS_INVALID_KEY_IDID is not a valid ID.
KEYSTORE_PSA_STATUS_COMMUNICATION_FAILUREThere was an failure in communication with the cryptoprocessor. The key material may still be present in the cryptoprocessor.
KEYSTORE_PSA_STATUS_STORAGE_FAILUREThe storage is corrupted. Implementations shall make a best effort to erase key material even in this stage, however applications should be aware that it may be impossible to guarantee that the key material is not recoverable in such cases.
KEYSTORE_PSA_STATUS_CORRUPTION_DETECTEDAn unexpected condition which is not a storage corruption or a communication failure occurred. The cryptoprocessor may have been compromised.
KEYSTORE_PSA_STATUS_BAD_STATEThe library has not been previously initialized by KeyStore_PSA_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ KeyStore_PSA_copyKey()

int_fast16_t KeyStore_PSA_copyKey ( KeyStore_PSA_KeyFileId  source_key,
KeyStore_PSA_KeyAttributes attributes,
KeyStore_PSA_KeyFileId target_key 
)

Make a copy of a key.

Copy key material from one location to another.

This function is primarily useful to copy a key from one location to another, since it populates a key using the material from another key which may have a different lifetime.

This function may be used to share a key with a different party, subject to implementation-defined restrictions on key sharing.

The policy on the source key must have the usage flag KEYSTORE_PSA_KEY_USAGE_COPY set. This flag is sufficient to permit the copy if the key has the lifetime KEYSTORE_PSA_KEY_LIFETIME_VOLATILE or KEYSTORE_PSA_KEY_LIFETIME_PERSISTENT. Some secure elements do not provide a way to copy a key without making it extractable from the secure element. If a key is located in such a secure element, then the key must have both usage flags KEYSTORE_PSA_KEY_USAGE_COPY and KEYSTORE_PSA_KEY_USAGE_EXPORT in order to make a copy of the key outside the secure element.

The resulting key may only be used in a way that conforms to both the policy of the original key and the policy specified in the attributes parameter:

  • The usage flags on the resulting key are the bitwise-and of the usage flags on the source policy and the usage flags in attributes.
  • If both allow the same algorithm or wildcard-based algorithm policy, the resulting key has the same algorithm policy.
  • If either of the policies allows an algorithm and the other policy allows a wildcard-based algorithm policy that includes this algorithm, the resulting key allows the same algorithm.
  • If the policies do not allow any algorithm in common, this function fails with the status KEYSTORE_PSA_STATUS_INVALID_ARGUMENT.

The effect of this function on implementation-defined attributes is implementation-defined.

Parameters
[in]source_keyThe key to copy. It must allow the usage KEYSTORE_PSA_KEY_USAGE_COPY. If a private or secret key is being copied outside of a secure element it must also allow KEYSTORE_PSA_KEY_USAGE_EXPORT.
[in]attributesThe attributes for the new key. They are used as follows:
  • The key type and size may be 0. If either is nonzero, it must match the corresponding attribute of the source key.
  • The key location (the lifetime and, for persistent keys, the key identifier) is used directly.
  • The policy constraints (usage flags and algorithm policy) are combined from the source key and attributes so that both sets of restrictions apply, as described in the documentation of this function.
[out]target_keyOn success, an identifier for the newly created key. For persistent keys, this is the key identifier defined in attributes. 0 on failure.
Return values
KEYSTORE_PSA_STATUS_SUCCESS
KEYSTORE_PSA_STATUS_INVALID_KEY_IDsource_key is invalid.
KEYSTORE_PSA_STATUS_ALREADY_EXISTSThis is an attempt to create a persistent key, and there is already a persistent key with the given identifier.
KEYSTORE_PSA_STATUS_INVALID_ARGUMENTThe lifetime or identifier in attributes are invalid, or the policy constraints on the source and specified in attributes are incompatible, or attributes specifies a key type or key size which does not match the attributes of the source key.
KEYSTORE_PSA_STATUS_NOT_PERMITTEDThe source key does not have the KEYSTORE_PSA_KEY_USAGE_COPY usage flag, or the source key is not exportable and its lifetime does not allow copying it to the target's lifetime.
KEYSTORE_PSA_STATUS_INSUFFICIENT_MEMORY
KEYSTORE_PSA_STATUS_INSUFFICIENT_STORAGE
KEYSTORE_PSA_STATUS_COMMUNICATION_FAILURE
KEYSTORE_PSA_STATUS_HARDWARE_FAILURE
KEYSTORE_PSA_STATUS_STORAGE_FAILURE
KEYSTORE_PSA_STATUS_CORRUPTION_DETECTED
KEYSTORE_PSA_STATUS_BAD_STATEThe library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale