ECDHLPF3HSM Object.
More...
#include <ECDHLPF3HSM.h>
ECDHLPF3HSM Object.
- Note
- The application must not access any member variables of this structure!
§ privateKey
const CryptoKey* ECDHLPF3HSM_Object::privateKey |
§ publicKey
§ sharedSecret
§ curveType
§ curveLength
§ domainId
§ curveFamily
Eip130Domain_ECCurveFamily_t ECDHLPF3HSM_Object::curveFamily |
§ callbackFxn
§ operation
§ operationType
§ returnBehavior
§ keyMaterialEndianness
§ accessTimeout
uint32_t ECDHLPF3HSM_Object::accessTimeout |
§ returnStatus
int_fast16_t ECDHLPF3HSM_Object::returnStatus |
§ hsmStatus
int_fast16_t ECDHLPF3HSM_Object::hsmStatus |
§ privateKeyAssetID
uint32_t ECDHLPF3HSM_Object::privateKeyAssetID |
§ publicKeyAssetID
uint32_t ECDHLPF3HSM_Object::publicKeyAssetID |
§ publicDataAssetID
uint32_t ECDHLPF3HSM_Object::publicDataAssetID |
§ paramAssetID
uint32_t ECDHLPF3HSM_Object::paramAssetID |
§ curveParam
const uint8_t* ECDHLPF3HSM_Object::curveParam |
§ curveParamSize
uint32_t ECDHLPF3HSM_Object::curveParamSize |
§ output
uint8_t ECDHLPF3HSM_Object::output[144] |
§ driverCreatedKeyAsset
bool ECDHLPF3HSM_Object::driverCreatedKeyAsset |
§ isOpen
bool ECDHLPF3HSM_Object::isOpen |
The documentation for this struct was generated from the following file: