![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.12.00
|
Data Fields | |
| uint8_t | antennaPermutationIndex |
| Antenna permutation index. More... | |
| modeTwoStepData_t | data [] |
| Array of length (numAntennaPath + 1), each element is of type modeTwoStepData_t. More... | |
| uint8_t | packetAntenna |
| PacKet antenna. More... | |
| uint8_t | packetNadm |
| Attack likelihood. More... | |
| uint8_t | packetQuality |
| Packet quality. More... | |
| uint8_t | packetRssi |
| Packet RSSI. More... | |
| uint16_t | ToDToA |
| Time difference in 0.5 ns units between arrival and departure of CS packets. More... | |
| uint8_t antennaPermutationIndex |
Antenna permutation index.
| modeTwoStepData_t data[] |
Array of length (numAntennaPath + 1), each element is of type modeTwoStepData_t.
| uint8_t packetAntenna |
PacKet antenna.
| uint8_t packetNadm |
Attack likelihood.
| uint8_t packetQuality |
Packet quality.
| uint8_t packetRssi |
Packet RSSI.
| uint16_t ToDToA |
Time difference in 0.5 ns units between arrival and departure of CS packets.