TI BLE5-Stack API Documentation  9.12.00
Data Fields
handoverSNParams_t Struct Reference

Host Handover Serving Node Configuration parameters. More...

Data Fields

uint16_t connHandle
 Connection handle. More...
 
uint32_t handoverDataSize
 The stack handover data size. More...
 
uint8_t handoverSnMode
 0 - Terminate the connection immediately on the serving node side, 1 - wait for the candidate response More...
 
uint16_t maxGattHandle
 Maximum GATT handle. More...
 
uint16_t minGattHandle
 Minimum GATT handle. More...
 
uint8_t * pHandoverData
 Pointer to the buffer the application allocated. More...
 
uint32_t rfu
 Reserved for future use. More...
 

Detailed Description

Host Handover Serving Node Configuration parameters.

Field Documentation

§ connHandle

uint16_t connHandle

Connection handle.

§ handoverDataSize

uint32_t handoverDataSize

The stack handover data size.

§ handoverSnMode

uint8_t handoverSnMode

0 - Terminate the connection immediately on the serving node side, 1 - wait for the candidate response

§ maxGattHandle

uint16_t maxGattHandle

Maximum GATT handle.

§ minGattHandle

uint16_t minGattHandle

Minimum GATT handle.

§ pHandoverData

uint8_t* pHandoverData

Pointer to the buffer the application allocated.

§ rfu

uint32_t rfu

Reserved for future use.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale