![]() |
![]() |
CC23x0R5DriverLibrary
|
#include "udma.h"
Functions | |
void | uDMAEnableChannelAttribute (uint32_t channelBitMask, uint32_t attr) |
Enables attributes of a uDMA channel. More... | |
void | uDMADisableChannelAttribute (uint32_t channelBitMask, uint32_t attr) |
Disables attributes of an uDMA channel. More... | |
uint32_t | uDMAGetChannelAttribute (uint32_t channelBitMask) |
Gets the enabled attributes of a uDMA channel. More... | |
void | uDMASetChannelControl (volatile uDMAControlTableEntry *pChannelControlStruct, uint32_t control) |
Sets the control parameters for a uDMA channel control structure. More... | |
void | uDMASetChannelTransfer (volatile uDMAControlTableEntry *pChannelControlStruct, uint32_t mode, void *pSrcAddr, void *pDstAddr, uint32_t transferSize) |
Sets the transfer parameters for a uDMA channel control structure. More... | |
uint32_t | uDMAGetChannelSize (volatile uDMAControlTableEntry const *pChannelControlStruct) |
Gets the current transfer size for a uDMA channel control structure. More... | |
uint32_t | uDMAGetChannelMode (volatile uDMAControlTableEntry const *pChannelControlStruct) |
Gets the transfer mode for a uDMA channel control structure. More... | |