Data Structures | Macros | Typedefs | Functions
EventP.h File Reference

Detailed Description

Event Group support.

============================================================================

Events are a collection of bits with an application-defined meaning, typically used for messaging or synchronisation. A task may check the state of a set of bits or pend on an EventP object to react to changes when they are posted from another context.

Only one Task may pend on a single EventP object at any given time.

Events are synchronous in nature, meaning that a receiving task will block or pend while waiting for the events to occur. When the desired events are received, the pending task continues its execution, as it would after a call to Semaphore_pend(), for example.

EventP_pend is used to wait for events. The eventMask determine which event(s) must occur before returning from EventP_pend. The timeout parameter allows the task to wait until a timeout, wait indefinitely, or not wait at all. If waitForAll is true, the pend call will not return until all of the bits in eventMask are set. If it is false, any of the bits in eventMask will be returned. A return value of zero indicates that a timeout has occurred. A non-zero return value is the set of events that were active at the time the task was unblocked. Event bits that caused a return (either the whole eventMask or any individual bit, depending on waitForAll) will be cleared when EventP_pend returns.


#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
Include dependency graph for EventP.h:

Go to the source code of this file.

Data Structures

union  EventP_Struct
 EventP structure. More...
 

Macros

#define EventP_STRUCT_SIZE   (52)
 Number of bytes greater than or equal to the size of any RTOS Event object. More...
 
#define EventP_WAIT_FOREVER   ~(0)
 Wait forever define. More...
 
#define EventP_NO_WAIT   (0)
 No wait define. More...
 

Typedefs

typedef union EventP_Struct EventP_Struct
 EventP structure. More...
 
typedef EventP_StructEventP_Handle
 Opaque client reference to an instance of a EventP. More...
 

Functions

EventP_Handle EventP_create (void)
 Create an EventP, allocating memory on the heap. More...
 
void EventP_delete (EventP_Handle handle)
 Function to delete an EventP. More...
 
EventP_Handle EventP_construct (EventP_Struct *obj)
 Construct an EventP, using statically allocated memory. More...
 
void EventP_destruct (EventP_Struct *obj)
 Function to destruct an EventP. More...
 
uint32_t EventP_pend (EventP_Handle event, uint32_t eventMask, bool waitForAll, uint32_t timeout)
 Wait for the events listed in eventMask. More...
 
void EventP_post (EventP_Handle event, uint32_t eventMask)
 Post events to an event object. More...
 
void EventP_clear (EventP_Handle event, uint32_t eventMask)
 Clear events from an event object. More...
 
uint32_t EventP_get (EventP_Handle event)
 Get the current events from an event object. More...
 

Macro Definition Documentation

§ EventP_STRUCT_SIZE

#define EventP_STRUCT_SIZE   (52)

Number of bytes greater than or equal to the size of any RTOS Event object.

BIOS 6.x: 20 BIOS 7.x: 20 FreeRTOS: 52

§ EventP_WAIT_FOREVER

#define EventP_WAIT_FOREVER   ~(0)

Wait forever define.

§ EventP_NO_WAIT

#define EventP_NO_WAIT   (0)

No wait define.

Typedef Documentation

§ EventP_Struct

EventP structure.

Opaque structure that should be large enough to hold any of the RTOS specific EventP objects.

§ EventP_Handle

Opaque client reference to an instance of a EventP.

A EventP_Handle returned from create or construct represents that instance.

Function Documentation

§ EventP_create()

EventP_Handle EventP_create ( void  )

Create an EventP, allocating memory on the heap.

EventP_create creates a new event object. EventP_create returns the handle of the new task object or NULL if the event could not be created.

When created, no bits of an event are set. For FreeRTOS, configSUPPORT_DYNAMIC_ALLOCATION also has to be set to 1 in FreeRTOSConfig.h. See 'Configuration with FreeRTOS' in the Core SDK User's Guide for how to do this.

This API cannot be called from interrupt contexts.

Return values
EventPhandle (NULL on failure)

§ EventP_delete()

void EventP_delete ( EventP_Handle  handle)

Function to delete an EventP.

Parameters
handleA EventP_Handle returned from EventP_create

§ EventP_construct()

EventP_Handle EventP_construct ( EventP_Struct obj)

Construct an EventP, using statically allocated memory.

EventP_construct creates a new event object. EventP_construct returns the handle of the new task object or NULL if the event could not be created.

When created, no bits of an event are set. For FreeRTOS, configSUPPORT_STATIC_ALLOCATION also has to be set to 1 in FreeRTOSConfig.h. See 'Configuration with FreeRTOS' in the Core SDK User's Guide for how to do this.

This API cannot be called from interrupt contexts.

Return values
EventPhandle (NULL on failure)

§ EventP_destruct()

void EventP_destruct ( EventP_Struct obj)

Function to destruct an EventP.

Parameters
objPointer to a EventP_Struct object that was passed to EventP_construct().
Returns

§ EventP_pend()

uint32_t EventP_pend ( EventP_Handle  event,
uint32_t  eventMask,
bool  waitForAll,
uint32_t  timeout 
)

Wait for the events listed in eventMask.

EventP_pend is used to wait for events. The eventMask determine which event(s) must occur before returning from EventP_pend. The timeout parameter allows the task to wait until a timeout, wait indefinitely, or not wait at all. If waitForAll is true, the pend call will not return until all of the bits in eventMask are set. If it is false, any of the bits in eventMask will be returned. A return value of zero indicates that a timeout has occurred. A non-zero return value is the set of events in the eventMask that were active at the time the task was unblocked.

Event bits that caused a return (either the whole eventMask or any individual bit, depending on waitForAll) will be cleared when EventP_pend returns.

A timeout value of EventP_WAIT_FOREVER causes the task to wait indefinitely for matching events to be posted. A timeout value of EventP_NO_WAIT causes EventP_pend to return immediately.

This API cannot be called from interrupt contexts.

Parameters
eventEvent handle
eventMaskMatch against the events in this bitmask. For FreeRTOS, only the 24 least significant bits in the event mask may be set, meaning the maximum allowed value for FreeRTOS is 0x00FFFFFF.
waitForAllIf true, only return when all matching bits are set
timeoutReturn after this many ClockP ticks, even if there is no match
Return values
Abitmask containing all consumed events, or zero on timeout.

§ EventP_post()

void EventP_post ( EventP_Handle  event,
uint32_t  eventMask 
)

Post events to an event object.

EventP_post() is used to signal events. If a task is waiting for the event and the event conditions are met, EventP_post() unblocks the task. If no tasks are waiting, EventP_post() simply registers the event with the event object and returns.

Parameters
eventEvent handle
eventMaskMask of eventIds to post (this must be non-zero). For FreeRTOS, only the 24 least significant bits in the event mask may be set, meaning the maximum allowed value for FreeRTOS is 0x00FFFFFF.

§ EventP_clear()

void EventP_clear ( EventP_Handle  event,
uint32_t  eventMask 
)

Clear events from an event object.

Clears the bits in eventMask from the EventP.

Parameters
eventEvent handle
eventMaskMask of eventIds to clear (this must be non-zero). For FreeRTOS, only the 24 least significant bits in the event mask may be set, meaning the maximum allowed value for FreeRTOS is 0x00FFFFFF.

§ EventP_get()

uint32_t EventP_get ( EventP_Handle  event)

Get the current events from an event object.

Returns the currently active events in an EventP without clearing them.

Parameters
eventEvent handle
Return values
Currentlyactive events
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale