![]() |
![]() |
Table entry that maps a virtual adc channel to the corresponding hardware configuration. More...
#include <ADCBufLPF3.h>
Data Fields | |
| uint_fast32_t | refVoltage |
| uint8_t | adcInputDIO |
| uint8_t | internalChannel |
| ADCLPF3_Reference_Source | refSource |
Table entry that maps a virtual adc channel to the corresponding hardware configuration.
| uint_fast32_t ADCBufLPF3_AdcChannelLutEntry::refVoltage |
Reference voltage of the selected reference source in microvolts
| uint8_t ADCBufLPF3_AdcChannelLutEntry::adcInputDIO |
DIO that this virtual channel is routed to. Should be set to GPIO_INVALID_INDEX if internal signal is used.
| uint8_t ADCBufLPF3_AdcChannelLutEntry::internalChannel |
Internal signal routed to ADC
| ADCLPF3_Reference_Source ADCBufLPF3_AdcChannelLutEntry::refSource |
Reference source for the ADC to use