![]() |
![]() |
BatMon Support Configuration. More...
#include <BatMonSupportLPF3.h>
Data Fields | |
| uint32_t | intNum |
| uint32_t | intPriority |
| uint32_t | intSubscriberId |
BatMon Support Configuration.
A sample structure is shown below:
| uint32_t BatMonSupportLPF3_Config::intNum |
Device-specific interrupt number. The interrupt must support the AON_PMU_COMB event.
| uint32_t BatMonSupportLPF3_Config::intPriority |
Device-specific interrupt priority
| uint32_t BatMonSupportLPF3_Config::intSubscriberId |
Device-specific interrupt subscriber ID, as defined in driverlib/evtsvt.h. This must match intNum.