Data Fields
ClockP_Params Struct Reference

Basic ClockP Parameters. More...

#include <ClockP.h>

Data Fields

bool startFlag
 
uint32_t period
 
uintptr_t arg
 

Detailed Description

Basic ClockP Parameters.

Structure that contains the parameters passed into ClockP_create() or ClockP_construct() when creating a ClockP instance. The ClockP_Params_init() function should be used to initialize the fields to default values before the application sets the fields manually. The ClockP default parameters are noted in ClockP_Params_init().

The default startFlag is false, meaning the user will have to call ClockP_start(). If startFlag is true, the clock instance will be started automatically when it is created.

The default value of period is 0, indicating a one-shot clock object. A non-zero period indicates the clock function will be called periodically at the period rate (in system clock ticks), after the clock is initially started and set to expire with the 'timeout' argument.

Field Documentation

§ startFlag

bool ClockP_Params::startFlag

Start immediately after instance is created.

§ period

uint32_t ClockP_Params::period

Period of clock object.

§ arg

uintptr_t ClockP_Params::arg

Argument passed to the clock function.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale