![]() |
![]() |
ECDSA software driver implementation for the Low Power F3 family.
============================================================================
This file should only be included in the board file to fill the ECDSA_config struct.
The driver is backed by a software ECC library implementation.
The driver implementation supports the following curves for ECDSA:
| Curves Supported |
|---|
| NISTP256 |
| NISTP224 |
#include <stdint.h>#include <stdbool.h>#include <ti/drivers/ECDSA.h>#include <third_party/ecc/include/lowlevelapi.h>
Go to the source code of this file.
Data Structures | |
| struct | ECDSALPF3SW_HWAttrs |
| ECDSALPF3SW Hardware Attributes. More... | |
| struct | ECDSALPF3SW_Object |
| ECDSALPF3SW Object. More... | |
Macros | |
| #define | ECDSALPF3SW_ECC_WINDOW_SIZE 3 |
| #define | ECDSALPF3SW_ECC_WORKZONE_WORDS 254 |
| #define ECDSALPF3SW_ECC_WINDOW_SIZE 3 |
| #define ECDSALPF3SW_ECC_WORKZONE_WORDS 254 |