Data Fields
AESCBC_Params Struct Reference

CBC Parameters. More...

#include <AESCBC.h>

Collaboration diagram for AESCBC_Params:
Collaboration graph
[legend]

Data Fields

AESCBC_ReturnBehavior returnBehavior
 
AESCBC_CallbackFxn callbackFxn
 
uint32_t timeout
 
void * custom
 

Detailed Description

CBC Parameters.

CBC Parameters used with the AESCBC_open() call. Default values for these parameters are set using AESCBC_Params_init().

See also
AESCBC_Params_init()

Field Documentation

§ returnBehavior

AESCBC_ReturnBehavior AESCBC_Params::returnBehavior

Blocking, callback, or polling return behavior

§ callbackFxn

AESCBC_CallbackFxn AESCBC_Params::callbackFxn

Callback function pointer

§ timeout

uint32_t AESCBC_Params::timeout

Timeout before the driver returns an error in AESCBC_RETURN_BEHAVIOR_BLOCKING

§ custom

void* AESCBC_Params::custom

Custom argument used by driver implementation


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale