![]() |
![]() |
AESCBCLPF3 Object. More...
#include <AESCBCLPF3.h>

Data Fields | |
| AESCommonLPF3_Object | common |
| volatile uint32_t | iv [AES_IV_LENGTH_BYTES/4] |
| const uint8_t * | input |
| uint8_t * | output |
| AESCBC_CallbackFxn | callbackFxn |
| AESCBC_OperationUnion * | operation |
| AESCBC_OperationType | operationType |
| bool | threadSafe |
| size_t | inputLength |
| int_fast16_t | hsmStatus |
| The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly. More... | |
| uint32_t | keyAssetID |
| KeyStore_PSA_KeyLocation | keyLocation |
| bool | segmentedOperationInProgress |
AESCBCLPF3 Object.
The application must not access any member variables of this structure!
| AESCommonLPF3_Object AESCBCLPF3_Object::common |
| volatile uint32_t AESCBCLPF3_Object::iv[AES_IV_LENGTH_BYTES/4] |
| const uint8_t* AESCBCLPF3_Object::input |
| uint8_t* AESCBCLPF3_Object::output |
| AESCBC_CallbackFxn AESCBCLPF3_Object::callbackFxn |
| AESCBC_OperationUnion* AESCBCLPF3_Object::operation |
| AESCBC_OperationType AESCBCLPF3_Object::operationType |
| bool AESCBCLPF3_Object::threadSafe |
| size_t AESCBCLPF3_Object::inputLength |
| int_fast16_t AESCBCLPF3_Object::hsmStatus |
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly.
| uint32_t AESCBCLPF3_Object::keyAssetID |
| KeyStore_PSA_KeyLocation AESCBCLPF3_Object::keyLocation |
| bool AESCBCLPF3_Object::segmentedOperationInProgress |