![]() |
![]() |
SHA2 Parameters. More...
#include <SHA2.h>

Data Fields | |
| SHA2_HashType | hashType |
| SHA2_ReturnBehavior | returnBehavior |
| SHA2_CallbackFxn | callbackFxn |
| uint32_t | timeout |
SHA2 Parameters.
SHA2 Parameters are used to with the SHA2_open() call. Default values for these parameters are set using SHA2_Params_init().
| SHA2_HashType SHA2_Params::hashType |
SHA2 variant to use. This determines the output digest length.
| SHA2_ReturnBehavior SHA2_Params::returnBehavior |
Blocking, callback, or polling return behavior
| SHA2_CallbackFxn SHA2_Params::callbackFxn |
Callback function pointer
| uint32_t SHA2_Params::timeout |
Timeout before the driver returns an error in SHA2_RETURN_BEHAVIOR_BLOCKING