xWRL684x MMWAVE-L-SDK  06.00.05
UART Echo

Note
Refer to XDS Firmware Update for using UARTA and DSS_SCIA

Introduction

This example demonstrates the UART RX and TX operation in blocking, interrupt mode of operation. This example receives 8 characters and echos back the same. The application ends when the user types 8 characters.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
Toolchain ti-arm-clang
Boards xWRL6844-evm
Example folder examples/drivers/uart/uart_echo/

Using SDK with SysConfig

A GUI tool SysConfig is used to configure different modules and peripherals of the example. Using this tool, users can select and customize different modules and peripherals. The SysConfig tool will generate the code for initializing and configuring these modules. This configuration is saved to a file called example.syscfg for every example. To know more about how to use SDK with SysConfig, Visit this page

Using SDK with SysConfig

Steps to Run the Example

See Also

UART

Sample Output

Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console. In UART console you need to enter 8 characters.

CCS Console:

[UART] Echo example started ...
All tests have passed!!

UART Console:

This is uart echo test blocking mode
Receives 8 characters then echo's back. Please input..
12345678
All tests have passed!!