3.11.3. Use Camera¶
The Camera Evaluation section briefly shows how to capture video using either a USB camera or a CSI-2 image sensor. This section will go further to explain how to configure the camera/sensor to capture videos at a specific format, resolution or frame rate. It will also be explained in this section how to enable a new CSI-2 sensor other than the default supported sensor in the SDK.
3.11.3.1. Query Camera Capabilities¶
Before configuring the camera/sensor, it is necessary to find out the supported formats, resolutions and frame rates.
3.11.3.1.1. Query a USB Camera¶
The v4l2-ctl
utility can be used to query a USB camera. Below commands show an
example of querying a USB camera.
Find the video device number of the camera:
# v4l2-ctl --list-devices Video Capture 4 (usb-xhci-hcd.1.auto-1.2): /dev/video1 /dev/video2 /dev/media1
Display the supported formats of the camera (using video1 listed above):
# v4l2-ctl --list-formats -d /dev/video1 ioctl: VIDIOC_ENUM_FMT Type: Video Capture [0]: 'YUYV' (YUYV 4:2:2) [1]: 'MJPG' (Motion-JPEG, compressed)
Display the supported resolutions (frame sizes) and frame rates for all formats:
# v4l2-ctl --list-formats-ext -d /dev/video1 ioctl: VIDIOC_ENUM_FMT Type: Video Capture [0]: 'YUYV' (YUYV 4:2:2) Size: Discrete 640x480 Interval: Discrete 0.033s (30.000 fps) Interval: Discrete 0.042s (24.000 fps) ... [1]: 'MJPG' (Motion-JPEG, compressed) Size: Discrete 640x480 Interval: Discrete 0.033s (30.000 fps) Interval: Discrete 0.042s (24.000 fps) Interval: Discrete 0.050s (20.000 fps)
3.11.3.1.2. Query a CSI-2 Image Sensor¶
For CSI-2 image sensors, instead of querying the video device, we need to query the
sensor’s device node. The reason is that the CSIRX subsystem (video device) has no
limitations on frame sizes. It is the image sensor (device node) that has limitations.
The media-ctl
utility will be used with the v4l2-ctl
utility to query the sensor.
A few steps are needed to find out the supported resolutions and frame rates, with
examples given below.
Find the media device number corresponding to the image sensor (note media0 below):
# v4l2-ctl --list-devices j721e-csi2rx (platform:30102000.ticsi2rx): ... /dev/media0
Find the device node name corresponding to the image sensor (using OV5640 as an example) (note /dev/v4l-subdev2 and pad0 below):
# media-ctl -d /dev/media0 -p Media controller API version 5.10.109 ... - entity 13: ov5640 4-003c (1 pad, 1 link) type V4L2 subdev subtype Sensor flags 0 device node name /dev/v4l-subdev2 pad0: Source [fmt:UYVY8_2X8/640x480@1/30 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range] -> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE] ...
List the media bus codes and find the one for the desired format:
# v4l2-ctl -d /dev/v4l-subdev2 --list-subdev-mbus-codes pad=0 ioctl: VIDIOC_SUBDEV_ENUM_MBUS_CODE (pad=0) 0x4001: MEDIA_BUS_FMT_JPEG_1X8 0x2006: MEDIA_BUS_FMT_UYVY8_2X8 ...
Display the supported resolutions for the desired format (using the pad number and the media bus code obtained earlier):
# v4l2-ctl -d /dev/v4l-subdev2 --list-subdev-framesizes pad=0,code=0x2006 ioctl: VIDIOC_SUBDEV_ENUM_FRAME_SIZE (pad=0) Size Range: 176x144 - 176x144 Size Range: 320x240 - 320x240 Size Range: 640x480 - 640x480 Size Range: 720x480 - 720x480 Size Range: 720x576 - 720x576 Size Range: 1024x768 - 1024x768 Size Range: 1280x720 - 1280x720 Size Range: 1920x1080 - 1920x1080 Size Range: 2592x1944 - 2592x1944
Display the supported frame rates for a specific format and frame size:
# v4l2-ctl -d /dev/v4l-subdev2 --list-subdev-frameintervals pad=0,width=640,height=480,code=0x2006 ioctl: VIDIOC_SUBDEV_ENUM_FRAME_INTERVAL (pad=0) Interval: 0.067s (15.000 fps) Interval: 0.033s (30.000 fps) Interval: 0.017s (60.000 fps)
3.11.3.2. Configure Camera Parameters¶
After the capabilities of a camera/sensor are known, we can configure the camera/sensor to capture with specific parameters such as format, resolution or frame rate.
For a USB camera, the parameters can be specified in the gst-launch
command.
For example, the following command captures video in raw format, with
frame size 1024x576, at frame rate 15 fps:
# gst-launch-1.0 v4l2src device="/dev/video1" ! video/x-raw, width=1024, height=576, framerate=15/1 ! kmssink driver-name=tidss
Another command shown below captures video in MPEG format, with frame size 1920x1080, at frame rate 30 fps:
# gst-launch-1.0 v4l2src device="/dev/video1" ! image/jpeg, width=1920, height=1080, framerate=30/1 ! jpegparse ! jpegdec ! kmssink driver-name=tidss
For a CSI-2 sensor, the capturing parameters have to be configured using media-ctl
before capturing.
For example, the following commands set the OV5640 image sensor to UYVY format, 1024x768 frame size, 30 fps:
# v4l2-ctl -d /dev/v4l-subdev2 --list-subdev-frameintervals pad=0,width=1024,height=768,code=0x2006 ioctl: VIDIOC_SUBDEV_ENUM_FRAME_INTERVAL (pad=0) Interval: 0.067s (15.000 fps) Interval: 0.033s (30.000 fps) # media-ctl --set-v4l2 "'ov5640 4-003c':0 [fmt:UYVY8_2X8/1024x768@1/30 field:none]"
Refer to the supported formats and the corresponding codes displayed by command v4l2-ctl -d /dev/v4l-subdev2 --list-subdev-mbus-codes
.
Use media-ctl -p
to verify the format, frame size and frame rate are configured properly:
# media-ctl -d /dev/media0 -p Media controller API version 5.10.109 ... - entity 13: ov5640 4-003c (1 pad, 1 link) type V4L2 subdev subtype Sensor flags 0 device node name /dev/v4l-subdev2 pad0: Source [fmt:UYVY8_2X8/1024x768@1/30 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range] -> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE]
Then run GStreamer
to capture video with the configured parameters:
# gst-launch-1.0 v4l2src device="/dev/video0" ! video/x-raw , width=1024, height=768, framerate=30/1 ! kmssink driver-name=tidss
3.11.3.3. Enable A New CSI-2 Sensor¶
The Processor SDK supports one or more camera sensors by default. Both the driver modules and the device tree overlays for the supported sensors are pre-built and included in the SDK. To enable a new CSI-2 sensor, the following listed steps are needed to build the driver and device tree on the host and copy to the target. The OV9281 sensor is used as an example in the given steps. Some steps can be skipped if the driver is already included in the SDK.
Add the sensor driver source code to drivers/media/i2c (path is relative to <sdk root>/board-support/linux-<version>):
drivers/media/i2c/ov9281.c
Add the sensor in drivers/media/i2c/Kconfig. For example:
config VIDEO_OV9281 tristate "OmniVision OV9281 sensor support" depends on GPIOLIB && VIDEO_V4L2 && I2C select MEDIA_CONTROLLER select VIDEO_V4L2_SUBDEV_API select V4L2_FWNODE help This is a Video4Linux2 sensor driver for the OmniVision OV9281 camera sensor.
Add the sensor driver to drivers/media/i2c/Makefile:
obj-$(CONFIG_VIDEO_OV9281) += ov9281.o
Enable the sensor in ti_config_fragments/v8_audio_display.cfg:
CONFIG_VIDEO_OV9281=m
Create a device tree overlay for the sensor and add to arch/arm64/boot/dts/ti:
arch/arm64/boot/dts/ti/k3-am625-sk-csi2-ov9281.dts
Add the device tree overlay to arch/arm64/boot/dts/ti/Makefile:
dtb-$(CONFIG_ARCH_K3) += k3-am625-sk-csi2-ov9281.dtbo
Generate the defconfig and rebuild kernel image, modules and device tree, according to instructions given in section Build Kernel:
$ ti_config_fragments/defconfig_builder.sh -t ti_sdk_arm64_release $ make ti_sdk_arm64_release_defconfig $ make Image modules dtbs
Install the newly built kernel image, modules and device tree overlay binary:
$ sudo cp arch/arm64/boot/Image <path to root of file system>/boot $ sudo cp arch/arm64/boot/dts/ti/k3-am625-sk-csi2-ov9281.dtbo <path to root of file system>/boot $ sudo make INSTALL_MOD_PATH=<path to root of file system> modules_install
Boot the EVM with the updated kernel and root filesystem. Apply the device tree overlay at U-Boot prompt:
=>setenv name_overlays k3-am625-sk-csi2-ov9281.dtbo =>saveenv =>boot
Verify the sensor is added using “v4l2-ctl” and “media-ctl” utilities as described earlier.
#media-ctl -d /dev/media0 -p ... - entity 13: ov9281 4-0060 (1 pad, 1 link) type V4L2 subdev subtype Sensor flags 0 device node name /dev/v4l-subdev2 pad0: Source [fmt:SGRBG8_1X8/1280x800 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range crop.bounds:(0,0)/1280x800 crop:(0,0)/1280x800] -> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE] ...