3.5. Root FilesystemΒΆ
The Processor SDK Linux package provides root filesystem (rootfs) images that contain programs, scripts, and Linux user-space components that abstract various hardware accelerators available in the SoC.
There are different filesystem images provided in the installed SDK under
folder filesystem/.
- tisdk-base-image
This is the barebone rootfs images, intended to be a starting point for users to add packages and create a custom rootfs that suits their project needs.
- tisdk-default-image
This is the complete rootfs image, that contains standard Linux commands and features. This image also contains the TI component libraries, binaries and out-of-box examples.
- tisdk-docker-rootfs-image
This is similar to tisdk-base-image, but has more packages included, such as Docker, WiFi/Bluetooth, Perl, and Pulseaudio, etc. It is intended to be used for docker container support.
- tisdk-tiny-image
This is a very small rootfs image, only a few MegaBytes, intended to be used as initramfs for the use cases such as flashing system image. It uses SysVinit rather than systemd as in other rootfs images, and it does not include kernel files such as kernel image, dtb, or kernel modules.
Two file formats are provided in the SDK for each of the rootfs image,
*.tar.xz and *.wic.xz.
- *.tar.xz
This is the tarball of the rootfs. It can be used to update the rootfs partition of a bootable SD Card, or setup the rootfs for NFS boot.
- *.wic.xz
This is the raw bootable Linux image containing both bootloaders and rootfs. This image can be directly written to an SD Card to create a Linux bootable SD Card. Refer to Create a Linux Bootable SD Card for details of the SD Card writing process.