EtherNet/IP™ Adapter  1.04.06
User Reference Manual
EI_API_ADP_MCAST_CONFIG_STR Struct Reference

General multicast attribute parameter collection. More...

#include <EI_API_def.h>

Data Fields

uint8_t i8uAllocControl
 Multicast address allocation control word. Determines how addresses are allocated. More...
 
uint8_t i8uReserved
 Reserved. More...
 
uint16_t i16uNumMcast
 Number of IP multicast addresses to allocate for EtherNet/IP. More...
 
uint32_t i32uMcastStartAddr
 Starting multicast address from which to begin allocation. More...
 

Detailed Description

General multicast attribute parameter collection.

IP multicast address configuration.