AWRL6844 CPD Users Guide

Table of Contents

Overview

This lab demonstrates the use of TI 60GHz mmWave sensors AWRL6844 for in-cabin sensing applications including Vehicle Intruder Detection (ID), Child Presence Detection (CPD) and Seat Belt Reminder (SBR). CPD and SBR will share the same signal processing chain for point cloud generation. Note that this lab is tested and tuned with AWRL6844EVM board and top front console mounting. Optimization effort will be needed to achieve best performance for other antenna design and other mounting position.

The same demo binary and visualizer will be used for all three applications, i.e., ID, CPD and SBR. Different configuration files can be loaded which enable the three different applications.

In this users guide, we will focus on the CPD application. Real-time demo recording clips are shown below to demonstrate the CPD performance in different test scenerios. The accumulated point clouds display across 30 frames. The blue box indicates a child is detected and the green box indicates an adult is detected. Currently, the classifier is per-seat based. A per-car decision can be added at visualizer level. Since we are moving the baby into different position with demo running continuously, users may observe some transition period in the probability figure in this video. There are some consistent false points around the car, which are the strong static reflections leaking to the non-zero Doppler bins and being picked up by the super sensitive CFAR. Usually, they are not significent enough to cause a false detection in the classifier.