Opus Library
|
Macros | |
#define | OPUS_ALLOC_FAIL |
#define | OPUS_BAD_ARG |
#define | OPUS_BUFFER_TOO_SMALL |
#define | OPUS_INTERNAL_ERROR |
#define | OPUS_INVALID_PACKET |
#define | OPUS_INVALID_STATE |
#define | OPUS_OK |
#define | OPUS_UNIMPLEMENTED |
#define OPUS_ALLOC_FAIL |
Memory allocation has failed
#define OPUS_BAD_ARG |
One or more invalid/out of range arguments
#define OPUS_BUFFER_TOO_SMALL |
Not enough bytes allocated in the buffer
#define OPUS_INTERNAL_ERROR |
An internal error was detected
#define OPUS_INVALID_PACKET |
The compressed data passed is corrupted
#define OPUS_INVALID_STATE |
An encoder or decoder structure is invalid or already freed
#define OPUS_OK |
No error
#define OPUS_UNIMPLEMENTED |
Invalid/unsupported request number