Opus Library
|
Opus reference implementation types.
Go to the source code of this file.
Macros | |
#define | opus_int int |
#define | opus_int64 long long |
#define | opus_int8 signed char |
#define | opus_uint unsigned int |
#define | opus_uint64 unsigned long long |
#define | opus_uint8 unsigned char |
Typedefs | |
typedef short | opus_int16 |
typedef int | opus_int32 |
typedef unsigned short | opus_uint16 |
typedef unsigned int | opus_uint32 |
#define opus_int int |
OPUS integer, used for counters, etc
#define opus_int64 long long |
OPUS long int
#define opus_int8 signed char |
OPUS signed char
#define opus_uint unsigned int |
OPUS unsigned integer, used for counters, etc
#define opus_uint64 unsigned long long |
OPUS unsigned long int
#define opus_uint8 unsigned char |
OPUS unsigned char
typedef short opus_int16 |
OPUS 16 bit integer
typedef int opus_int32 |
OPUS 32 bit integer
typedef unsigned short opus_uint16 |
OPUS 16 bit unsigned integer
typedef unsigned int opus_uint32 |
OPUS 32 bit unsigned integer