Specifies a RF core firmware configuration. More...
#include <RF.h>
Data Fields | |
uint8_t | rfMode |
Specifies which PHY modes should be activated. Must be set to RF_MODE_MULTIPLE for dual-mode operation. More... | |
void(* | cpePatchFxn )(void) |
Pointer to CPE patch function. More... | |
void(* | mcePatchFxn )(void) |
Pointer to MCE patch function. More... | |
void(* | rfePatchFxn )(void) |
Pointer to RFE patch function. More... | |
Specifies a RF core firmware configuration.
RF_Mode selects a mode of operation and points to firmware patches for the RF core. There exists one instance per radio PHY configuration, usually generated by SmartRF Studio. After assigning RF_Mode configuration to the RF driver via RF_open(), the driver caches the containing information and re-uses it on every power-up.
uint8_t RF_Mode::rfMode |
Specifies which PHY modes should be activated. Must be set to RF_MODE_MULTIPLE for dual-mode operation.
void(* RF_Mode::cpePatchFxn) (void) |
Pointer to CPE patch function.
void(* RF_Mode::mcePatchFxn) (void) |
Pointer to MCE patch function.
void(* RF_Mode::rfePatchFxn) (void) |
Pointer to RFE patch function.