RF commands reference¶
Please find a detailed description for each command in the Radio chapter of the CC13x0 CC26x0 SimpleLink Wireless MCU Technical Reference Manual.
Protocol-Independent Direct Commands¶
Command name |
Description |
---|---|
CMD_ABORT |
Abort a running radio operation command immediately. |
CMD_GET_RSSI |
Read the current RSSI while an RX command is running. |
CMD_PING |
Respond with an interrupt event. |
CMD_START_RAT |
Start the RAT without synchronization to the RTC. |
CMD_STOP |
Abort a running radio operation command at the next possibility. |
Protocol-Independent Immediate Commands¶
Command name |
Description |
---|---|
CMD_ARM_RAT_CH |
Enable counting for a given RAT channel. |
CMD_BUS_REQUEST |
Set or reset a dependency on the system bus. |
CMD_DISABLE_RAT_CH |
Disable RAT channel. |
CMD_DISARM_RAT_CH |
Disable counting for a given RAT channel. |
CMD_GET_FW_INFO |
Request information about the RF core firmware. |
CMD_READ_RFREG |
Read a register on the RF core and return its value. |
CMD_SET_RAT_CMP |
Set a RAT channel into compare mode and load the comparison register. |
CMD_SET_RAT_CPT |
Set a RAT channel into capture mode and configure a capture input. |
CMD_SET_RAT_OUTPUT |
Set the operation mode for a RAT channel output. |
CMD_SET_TX_POWER |
Update the TX output power to a new value. |
CMD_SET_TX20_POWER |
Set Transmit Power of the 20-dBm PA. |
CMD_TRIGGER |
Fire a trigger in a currently running radio operation. |
Set new synthesizer frequency without doing a re-calibration. |
|
CMD_UPDATE_RADIO_SETUP |
Execute a set of register overrides. |
Immediate Commands for Data Queue Manipulation¶
Command name |
Description |
---|---|
CMD_ADD_DATA_ENTRY |
Add Data Entry to Queue. |
CMD_REMOVE_DATA_ENTRY |
Remove First Data Entry From Queue. |
CMD_FLUSH_QUEUE |
Flush Queue. |
CMD_CLEAR_RX |
Clear All RX Queue Entries. |
CMD_REMOVE_PENDING_ENTRIES |
Remove Pending Entries From Queue. |
Protocol-Independent Radio Operation Commands¶
Command name |
Description |
---|---|
CMD_NOP |
The command only waits for the start trigger, and then ends. |
CMD_RADIO_SETUP |
Set Up Radio Settings Command. |
CMD_FS_POWERUP |
Power Up Frequency Synthesizer. |
CMD_FS_POWERDOWN |
Power Down Frequency Synthesizer. |
CMD_FS |
Set the synthesizer frequency. |
CMD_FS_OFF |
Turn Off Frequency Synthesizer. |
CMD_RX_TEST |
Set the RF core into receive state without using the CPE. |
CMD_TX_TEST |
Send a modulated or unmodulated test signal. |
CMD_SYNC_STOP_RAT |
Stop the RAT and save its state. |
CMD_SYNC_START_RAT |
(Re-)start the RAT and synchronize it to the RTC. |
CMD_COUNT |
Count the own execution. |
CMD_SCH_IMM |
Wrap a direct or immediate command in a radio operation. |
CMD_COUNT_BRANCH |
Branch to alternative commands based on a counter value. |
CMD_PATTERN_CHECK |
Compare an arbitrary memory location to a given pattern. |
Prop Radio Operation Commands¶
Command name |
Description |
---|---|
Carrier sense. Monitor the RF activity on a RF channel. |
|
CMD_PROP_RADIO_DIV_SETUP |
Setup the RF core into proprietary mode in the Sub-1 GHz band. |
CMD_PROP_RADIO_SETUP |
Setup the RF core into proprietary mode in the 2.4 GHz band. |
CMD_PROP_RESTART_RX |
Stop receiving the current packet and go back to sync search. |
CMD_PROP_RX |
Receive one or multiple packets in proprietary mode (simple format). |
Receive one or multiple packets in proprietary mode (advanced format). |
|
CMD_PROP_RX_SNIFF |
Do carrier sense and receive one or multiple packets in proprietary mode (simple format). |
CMD_PROP_RX_ADV_SNIFF |
Do carrier sense and receive one or multiple packets in proprietary mode (advanced format). |
CMD_PROP_SET_LEN |
Set the length of packet while the packet is being received. |
CMD_PROP_TX |
Send one packet in proprietary mode (simple format). |
CMD_PROP_TX_ADV |
Send one packet in proprietary mode (advanced format). |
IEEE Radio Operation Commands¶
Command name |
Description |
---|---|
CMD_IEEE_RX |
Run receiver. |
CMD_IEEE_ED_SCAN |
Run energy detect scan. |
CMD_IEEE_TX |
Transmit packet. |
CMD_IEEE_CSMA |
Perform CSMA-CA. |
CMD_IEEE_RX_ACK |
Receive acknowledgment. |
CMD_IEEE_ABORT_BG |
ABORT background level operation. |
CMD_FG_SCH_IMM |
Behaves as CMD_SCH_IMM. |
CMD_IEEE_MOD_CCA |
Modify CCA parameters for running receiver. |
CMD_IEEE_MOD_FILT |
Modify frame filtering parameters for running receiver. |
CMD_IEEE_MOD_SRC_MATCH |
Modify source matching parameters for running receiver. |
CMD_IEEE_ABORT_FG |
ABORT foreground level operation. |
CMD_IEEE_STOP_FG |
Stop foreground level operation. |
CMD_IEEE_CCA_REQ |
Request CCA and RSSI information. |
High Speed (HS) Radio Operation Commands¶
Command name |
Description |
---|---|
CMD_HS_TX |
High-Speed Transmit Command. |
CMD_HS_RX |
High-Speed Receive Command. |