Common User Interface

It is recommended to use PuTTY as the serial terminal program for these sample applications because the serial output has been verified to be formatted correctly in this program. For serial port setup, select 115200 for baud rate and disable flow control.

The user interface allows to control the network configuration as well as application behavior. The network interface is common for all applications and is implemented in the module ssf.c on the sensor application and csf.c on the collector application. The application specifics of the serial interface is implemented in its respective application files.

The user interface consists of a series of circular menus that are navigated with the arrow keys. Pressing the Enter key will enter submenu. Use the up and down arrow keys to change the parameters on the menu (eg. channel mask, PAN ID, install codes, etc.).

The common user interface is also dependent on the capabilities of the compiled device, e.g. Collector devices (coordinators) will be able to open/close the network, whereas sensor devices will only require to start the sensor.

The common user interface also allows interaction with the specific application menu system under the App menu screen.

Welcome and <Help> Screens

The Welcome Screen (Figure 17.) displays the application name and leads to the Help Screen (Figure 18.), which outlines the generic functionality of the keys throughout the application. The following sections describe the specific functionality of the keys for each menu screen.

../_images/Welcome-screen.png

Figure 17. Welcome screen

../_images/Help-screen.png

Figure 18. Help screen

Welcome and Help Screens

Key

Functionality

Comment

Left/Right Arrow Keys

Menu navigation

Move to previous/next screen

Enter

Help

Press Enter to show the help screen, press Enter again to go back to the Welcome Screen

Information Screen

The lower portion of the screen (Figure 19.) displays various information about the device. about the device such as the IEEE address, the PAN ID, the channel, short address, logical device type, and the parent short address.

../_images/Info-screen.png

Figure 19. Info screen example

Status

The Device Info field shows information about the device (e.g. Waiting, starting, started, joined, orphaned, etc.).

Mode:

  • NBCN - Non-Beacon Mode

  • BCN - Beacon Mode

  • FH - Frequency Hopping Mode

Addr:

  • Device Short Address (Assigned by the Collector device)

PanId:

  • 16-bit PAN ID which this device is part of

Ch:

  • Logical channel of the network

PermitJoin (On Collector devices only):

  • Status of the network, is it open or closed.

Device Status

The Device Status line will show the latest information coming in, for example if the sensor just reported its temperature you will see it in this line like so (Figure 20.).

This message is modifiable to show what your application needs, but below you can see the default view for a temperature sensor.

../_images/Device.png

Figure 20. Device Status example

Addr

  • 16-bit NWK address of the device

Temp:

  • Internal temperature of your sensor device

RSSI:

  • Received Signal Strength Indicator.

Number of Joined Devices

The number of devices currently connected to the NWK.

<Configure> Menu

The Configure Menu (Figure 21.) contains several sub-menus that allow the user to manipulate the NWK Key, channel masks and PAN ID. This configuration will define the device behavior during BDB commissioning procedures.

../_images/Configure-Menu.png

Figure 21. Configure Menu

Channel Mask Screen

The Channel Mask Screen (Figure 22.) display and allow modification of the default channel configuration of the device for channel mask. Channel mask is a Bit-Masked value, for example if you have 0F 00 00 00 it means you have channels 0-3 enabled, or if you have F0 0F 00 00 it means you have channels 4-11 enabled. Press the Enter key to start changing the mask, highlight the value you want to modify and type in the value you want in Hex (0-F).

../_images/Channel-Mask.png

Figure 22. Channel Mask Screen

<Channel Mask> – view mode

Key

Functionality

Comment

Left/Right

Menu navigation

Move to previous/next screen

Enter

Select

Enter edit mode

<Channel Mask> – edit mode

Key

Functionality

Comment

Left/Right

Menu navigation

Move to previous/next screen

Enter

Select

Enter edit mode

0-F

Modify Value

Modify Channel Mask

<PAN ID> Screen

The PAN ID Screen (Figure 23.) allows changing of the default PAN ID (0xFFFF by default) to any desired value.

../_images/PAN-ID.png

Figure 23. PAN ID Screen - view mode

<PAN ID> Screen – view mode

Key

Functionality

Comment

Left/Right

Menu navigation

Move to previous/next screen

Enter

Select

Enter edit mode

<PAN ID> Screen – edit mode

Key

Functionality

Comment

Left/Right

Digit navigation

Move to previous/next digit

0-F

Value change

Change the value of the highlighted digit

Enter

Select

Save and exit mode

Set NWK Key

The SET NWK KEY Screen (Figure 24.) allows changing of the default NWK Security Key to any desired value.

Note

That the device will need to have been flashed with the secured Lib (CCS does this by default), and both the sensor and collector device must share the NWK Key.

../_images/SET-NWK-KEY.png

Figure 24. SET-NWK-KEY Screen - view mode

<Set NWK Key> Screen – view mode

Key

Functionality

Comment

Left/Right

Menu navigation

Move to previous/next screen

Enter

Select

Enter edit mode

<Set NWK Key> Screen – edit mode

Key

Functionality

Comment

Left/Right

Digit navigation

Move to previous/next digit

0-F

Value change

Change the value of the highlighted digit

Enter

Select

Save and exit mode

Network Actions

The Network actions Screens (Figure 25., Figure 26., Figure 27., Figure 28., Figure 29., Figure 30.)allow enabling/disabling of the top level commissioning procedures that will be performed when the collector and sensor devices have started and ready to join a network.

../_images/Network-Actions.png

Figure 25. Network-Actions Screen

FORM NWK

The FORM NWK action is available for a collector device of our 15.4 Stack network. This actions will allow the collector to start the network, it is the first step to get TI15.4 stack network going.

../_images/FORM-NWK.png

Figure 26. FORM-NWK Screen

OPEN NWK

The OPEN NWK action is available for a collector device of our 15.4 Stack network. This actions will allow the collector to open the network after being started, it is the second step to get TI15.4 stack network going, at this point a sensor device will be able to join.

../_images/OPEN-NWK.png

Figure 27. OPEN-NWK Screen

CLOSE NWK

The CLOSE NWK action is available for a collector device of our 15.4 Stack network. This actions will allow the collector to close the network after being opened, it is used when the collector will no longer accept new connections in the network.

../_images/CLOSE-NWK.png

Figure 28. CLOSE-NWK Screen

ASSOCIATE

The Associate action is available for a sensor device of our 15.4 Stack network. This actions will allow the sensor to scan and look for a network after being opened, it is used when the collector has already started a network and opened the network to new connections.

../_images/ASSOCIATE.png

Figure 29. ASSOCIATE Screen

DISASSOCIATE

The Disassociate action is available for a sensor device of our 15.4 Stack network. This actions will disassociate the sensor from a network after joining it.

../_images/DISASSOCIATE.png

Figure 30. DISASSOCIATE Screen

<Back> Screen

The Back Screen (Figure 31.) allows returning to the previous screen. When the back action is performed the upper level screen will be displayed automatically.

../_images/Back-Screen.png

Figure 31. Back Screen

<Back> Screen

Key

Functionality

Comment

Left/Right

Menu navigation

Move to previous/next screen

Enter

Select

Back to upper menu

<App> Menu

The App menu (Figure 32.) is application specific and will contain the menus to interact with the specific application implementation. Those specific application menus are explained in the README documentation provided by each application and referred in Example Applications.

This menu is intended to be used once the device is already associated to a network, as it provides ways to interact with the other devices in the network. For example, the Collector application will have a Send Toggle interface which will trigger the Sensor application Toggle its RED LED.

../_images/App-screen.png

Figure 32. App Screen

<App> Menu

Key

Functionality

Comment

Left/Right

Menu navigation

Move to previous/next screen

Enter

Select

Application specific action