Functions
Board.h File Reference

Detailed Description

Portable board-specific symbols.


The Board header file should be included in an application as follows:

#include "Board.h"

This header serves as device-independent interface for applications using peripherals connected to the device via standard digital interfaces; e.g, GPIO, SPI, I2C, UART, etc. Its purpose is to enable application code that references a peripheral to be portable to any device and board that supports the peripheral.

Usage

Synopsis

#include "Board.h"
void main(void)
{
:
}

Initializing the hardware

Board_init() must be called before any other driver API. This function calls the device specific initialization code that is required to as soon as possible after a device reset; e.g., to initialize clocks and power management functionality.

Portable peripheral usage

Each driver module declares symbols in Board.h that, if used, will improve code portability between both different devices and boards.

For example, the I2C driver adds Board.h symbol definitions of the form

Go to the source code of this file.

Functions

void Board_init (void)
 Performs "early" board-level initialization required by TI-DRIVERS. More...
 

Function Documentation

§ Board_init()

void Board_init ( void  )

Performs "early" board-level initialization required by TI-DRIVERS.

Board_init() must be called before any other TI-DRIVER API. This function calls all device and board specific initialization functions needed by TI-DRIVERS; e.g., to initialize clocks and power management functionality.

This function should only be called once and as early in the application's startup as possible. In most applications, a call to Board_init() is the first statement in main().

Precondition
Board_init must be called after every CPU reset and prior to enabling any interrupts.
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale