Data Fields
CryptoKey_KeyBlob_ Struct Reference

Keyblob CryptoKey datastructure. More...

#include <CryptoKey.h>

Data Fields

uint8_t * keyBlob
 
uint32_t keyBlobLength
 

Detailed Description

Keyblob CryptoKey datastructure.

This structure contains all the information necessary to access keying material stored in an encrypted structure in flash or RAM.

Field Documentation

§ keyBlob

uint8_t* CryptoKey_KeyBlob_::keyBlob

§ keyBlobLength

uint32_t CryptoKey_KeyBlob_::keyBlobLength

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale