Z-Stack API Reference  4.30.00.21
_gpdCommissioningCmd_t Struct Reference

Data Fields

uint8_t deviceId
 The DeviceID for GPD.
 
gpdCommissioningOptions_t options
 Options field.
 
gpdCommissioningExtOptions_t extOptions
 Extended options field.
 
uint8_t gpdKey [SEC_KEY_LEN]
 The security key for the GPD.
 
uint32_t gpdKeyMic
 Key MIC.
 
uint32_t gpdOutCounter
 Security frame counter.
 
gpdCommissioningAppInfo_t appInfo
 Application information.
 
uint16_t manufacturerId
 ManufacturerID value.
 
uint16_t modeId
 ModelID value.
 
uint8_t numberOfGpdCommands
 
uint8_t * pGpdCommandList
 Commmand list.
 
gpdCommissioningClusterLength_t clusterListLength
 Cluster list lenght.
 
uint16_t * pServerList
 Server list.
 
uint16_t * pClientList
 Client list.
 

Field Documentation

§ numberOfGpdCommands

uint8_t numberOfGpdCommands

Number of GP commands defines the number of items in the GP command list field.


The documentation for this struct was generated from the following file: