Z-Stack API Reference  4.30.00.21
zclDoorLockGetHolidayScheduleRsp_t Struct Reference

Client Commands Received: Get Holiday Schedule Response. More...

#include <zcl_closures.h>

Data Fields

uint8_t holidayScheduleID
 //!< Holiday Schedule ID number is between 0 - [# of Holiday Schedules Supported attribute].
 
uint8_t status
 //!< Request status
 
uint32_t zigBeeLocalStartTime
 Start time and end time are given in LocalTime.
 
uint32_t zigBeeLocalEndTime
 End of Holiday time.
 
uint8_t operatingModeDuringHoliday
 as listed in operating mode attribute. More...
 

Detailed Description

Client Commands Received: Get Holiday Schedule Response.

Field Documentation

§ operatingModeDuringHoliday

uint8_t operatingModeDuringHoliday

as listed in operating mode attribute.

Operating Mode is valid enumeration value


The documentation for this struct was generated from the following file: