TI BLE5-Stack API Documentation  2.02.00.01
Macros

Macros

#define ATT_ERROR_RSP   0x01
 ATT Error Response. This method is passed as a gattMsgEvent_t defined as attErrorRsp_t.
 
#define ATT_EXCHANGE_MTU_REQ   0x02
 ATT Exchange MTU Request. This method is passed as a GATT message defined as attExchangeMTUReq_t.
 
#define ATT_EXCHANGE_MTU_RSP   0x03
 ATT Exchange MTU Response. This method is passed as a GATT message defined as attExchangeMTURsp_t.
 
#define ATT_EXECUTE_WRITE_REQ   0x18
 ATT Execute Write Request. This method is passed as a GATT message defined as attExecuteWriteReq_t.
 
#define ATT_EXECUTE_WRITE_RSP   0x19
 ATT Execute Write Response. This method is passed as a GATT message defines as attErrorRsp_t.
 
#define ATT_FIND_BY_TYPE_VALUE_REQ   0x06
 ATT Find By Type Value Request. This method is passed as a GATT message defined as attFindByTypeValueReq_t.
 
#define ATT_FIND_BY_TYPE_VALUE_RSP   0x07
 ATT Find By Type Value Response. This method is passed as a GATT message defined as attFindByTypeValueRsp_t.
 
#define ATT_FIND_INFO_REQ   0x04
 ATT Find Information Request. This method is passed as a GATT message defined as attFindInfoReq_t.
 
#define ATT_FIND_INFO_RSP   0x05
 ATT Find Information Response. This method is passed as a GATT message defined as attFindInfoRsp_t.
 
#define ATT_HANDLE_VALUE_CFM   0x1e
 ATT Handle Value Confirmation. This method is passed as a GATT message.
 
#define ATT_HANDLE_VALUE_IND   0x1d
 ATT Handle Value Indication. This method is passed as a GATT message defined as attHandleValueInd_t.
 
#define ATT_HANDLE_VALUE_NOTI   0x1b
 ATT Handle Value Notification. This method is passed as a GATT message defined as attHandleValueNoti_t.
 
#define ATT_PREPARE_WRITE_REQ   0x16
 ATT Prepare Write Request. This method is passed as a GATT message defined as attPrepareWriteReq_t.
 
#define ATT_PREPARE_WRITE_RSP   0x17
 ATT Prepare Write Response. This method is passed as a GATT message defined as attPrepareWriteRsp_t.
 
#define ATT_READ_BLOB_REQ   0x0c
 ATT Read Blob Request. This method is passed as a GATT message defined as attReadBlobReq_t.
 
#define ATT_READ_BLOB_RSP   0x0d
 ATT Read Blob Response. This method is passed as a GATT message defined as attReadBlobRsp_t.
 
#define ATT_READ_BY_GRP_TYPE_REQ   0x10
 ATT Read By Group Type Request. This method is passed as a GATT message defined as attReadByGrpTypeReq_t.
 
#define ATT_READ_BY_GRP_TYPE_RSP   0x11
 ATT Read By Group Type Response. This method is passed as a GATT message defined as attReadByGrpTypeRsp_t.
 
#define ATT_READ_BY_TYPE_REQ   0x08
 ATT Read By Type Request. This method is passed as a GATT message defined as attReadByTypeReq_t.
 
#define ATT_READ_BY_TYPE_RSP   0x09
 ATT Read By Type Response. This method is passed as a GATT message defined as attReadByTypeRsp_t.
 
#define ATT_READ_MULTI_REQ   0x0e
 ATT Read Multiple Request. This method is passed as a GATT message defined as attReadMultiReq_t.
 
#define ATT_READ_MULTI_RSP   0x0f
 ATT Read Multiple Response. This method is passed as a GATT message defined as attReadMultiRsp_t.
 
#define ATT_READ_REQ   0x0a
 ATT Read Request. This method is passed as a GATT message defined as attReadReq_t.
 
#define ATT_READ_RSP   0x0b
 ATT Read Response. This method is passed as a GATT message defined as attReadRsp_t.
 
#define ATT_SIGNED_WRITE_CMD   0xD2
 ATT Signed Write Command.
 
#define ATT_UNSUPPORTED_METHOD   0x20
 Garbage ATT opcode used for negative testing.
 
#define ATT_WRITE_CMD   0x52
 ATT Write Command.
 
#define ATT_WRITE_REQ   0x12
 ATT Write Request. This method is passed as a GATT message defined as attWriteReq_t.
 
#define ATT_WRITE_RSP   0x13
 ATT Write Response. This method is passed as a GATT message.
 

Detailed Description

© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale