TI BLE5-Stack API Documentation
2.02.00.01
|
Data type of the first argument passed to the entry point of an image which contains a remote task. More...
Data Fields | |
ICall_Dispatcher | dispatch |
ICall dispatcher. | |
ICall_EnterCS | entercs |
enter CS | |
ICall_LeaveCS | leavecs |
leave CS | |
Data type of the first argument passed to the entry point of an image which contains a remote task.