TI BLE5-Stack API Documentation  2.02.00.01
Data Fields
hciEvt_DevInfo_t Struct Reference

LE Advertising Report Event. More...

Data Fields

uint8 addr [B_ADDR_LEN]
 device address
 
uint8 addrType
 public or random address type
 
uint8 dataLen
 length of report data
 
uint8 eventType
 advertisement or scan response event type
 
uint8 rspData [B_MAX_ADV_LEN]
 report data given by dataLen
 
int8 rssi
 report RSSI
 

Detailed Description

LE Advertising Report Event.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale