TI-OpenThread  1.08.02.01
Functions
CC1352P_4_LAUNCHXL/thread/thermostat/otsupport/otinstance.h File Reference
#include <openthread/instance.h>
+ Include dependency graph for CC1352P_4_LAUNCHXL/thread/thermostat/otsupport/otinstance.h:
+ This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Functions

otInstance * OtInstance_get (void)
 

Function Documentation

§ OtInstance_get()

otInstance* OtInstance_get ( void  )

Get a pointer to the OpenThread instance object.

Returns
Pointer to the OpenThread instance object.

Documented in otsupport/otinstance.h.

© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale