Running Software Examples on the CC13x1x or CC26x1x

Porting Software Examples for the CC13x1x or CC26x1x

The CC13x1x or CC26x1x is pin compatible with their respective CC13x2x1 or CC26x2x1 devices but with only one UART and SSI, 32KB + 8KB GP cache SRAM (with parity removed), and 40 kB of ROM. The following features and peripherals have also been removed entirely:

  • IEEE 754-compliant single-precision Floating Point Unit (FPU)
  • Memory Protection Unit (MPU)
  • AES 256-bit crypto accelerator
  • ECC and RSA Public Key Hardware Accelerator
  • SHA2 Accelerator
  • Sensor Controller with 4KB of SRAM

It is not possible to use the Migrating Board Variant tool to change the device types of projects using CC13x2x1 or CC26x2x1 to CC13x1x or CC26x1x. Developers are strongly encouraged to import a project which contains the correct settings for their target device and port the stack application accordingly. Example projects can be found from the following location:

<SDK_DIR>\examples\rtos\<LaunchPad variant>\<stack>\<application>\tirtos\<ccs/iar>

Choosing LaunchPad for Development

All LaunchPads currently use CC13x2x1 or CC26x2x1 devices, which developers are encouraged to evaluate with until acquiring CC13x1x or CC26x1x hardware. The following should be accounted for when starting development using CC13x2x1 or CC26x2x1 projects with the intent of migrating to the CC13x1x or CC26x1x:

  • RAM_SIZE defined in cc26x2lp.cmd should be reduced from 0x14000 to 0x8000 to account for the SRAM reduction. FLASH_SIZE should likewise be reduced from 0x52000 to 0x42000 since the BLE and 15.4 stacks will be moved from ROM to Flash to account for the decrease in ROM. This is a worst-case scenario as additional flash requirements range from ~28 to 63 kB based on application
  • Follow all Using the Cache as RAM instructions and disable NVOCMP_GPRAM in nvocmp.c (only pertaining to projects using the multi-page NV driver). Be aware that the program will need to run at a slightly reduced speed which will increase the device power consumption in sleep as noted in the User’s Guide. This difference can be further investigated using the Power Consumption → Power Modes table in the device datasheet

Beyond these feasible software changes, it should be noted that additional radio patches are required for the CC13x1x or CC26x1x that cannot be emulated with a CC13x2x1 or CC26x2x1 device. These changes are not expected to have a significant effect on radio performance and are thus inconsequential for initial evaluations.

The on-board devices can be swapped for the desired variant since they are pin compatible. As mentioned in the previous section, the correct example project must be selected for the specific device being used.

Moving From LaunchPad to Custom Board

You can find instructions on how to design and configure a custom board in the Custom Hardware chapter.