TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_devicedescriptor Struct Reference

#include <api_mac.h>

Data Fields

uint16_t panID
 
uint16_t shortAddress
 
ApiMac_sAddrExt_t extAddress
 

Detailed Description

Device Descriptor

Field Documentation

§ panID

uint16_t _apimac_devicedescriptor::panID

The 16-bit PAN identifier of the device

§ shortAddress

uint16_t _apimac_devicedescriptor::shortAddress

The 16-bit short address of the device

§ extAddress

ApiMac_sAddrExt_t _apimac_devicedescriptor::extAddress

The 64-bit IEEE extended address of the device. This element is also used inunsecuring operations on incoming frames.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale