TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_keyidlookupdescriptor Struct Reference

#include <api_mac.h>

Data Fields

uint8_t lookupData [APIMAC_MAX_KEY_LOOKUP_LEN]
 
uint8_t lookupDataSize
 

Detailed Description

Key ID Lookup Descriptor

Field Documentation

§ lookupData

uint8_t _apimac_keyidlookupdescriptor::lookupData[APIMAC_MAX_KEY_LOOKUP_LEN]

Data used to identify the key

§ lookupDataSize

uint8_t _apimac_keyidlookupdescriptor::lookupDataSize

0x00 indicates 5 octets; 0x01 indicates 9 octets


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale