TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_mcpsdatacnf Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_status_t status
 
uint8_t msduHandle
 
uint32_t timestamp
 
uint16_t timestamp2
 
uint8_t retries
 
uint8_t mpduLinkQuality
 
uint8_t correlation
 
int8_t rssi
 
uint32_t frameCntr
 

Detailed Description

MCPS data confirm type

Field Documentation

§ status

ApiMac_status_t _apimac_mcpsdatacnf::status

Contains the status of the data request operation

§ msduHandle

uint8_t _apimac_mcpsdatacnf::msduHandle

Application-defined handle value associated with the data request

§ timestamp

uint32_t _apimac_mcpsdatacnf::timestamp

The time, in backoffs, at which the frame was transmitted

§ timestamp2

uint16_t _apimac_mcpsdatacnf::timestamp2

The time, in internal MAC timer units, at which the frame was transmitted

§ retries

uint8_t _apimac_mcpsdatacnf::retries

The number of retries required to transmit the data frame

§ mpduLinkQuality

uint8_t _apimac_mcpsdatacnf::mpduLinkQuality

The link quality of the received ack frame

§ correlation

uint8_t _apimac_mcpsdatacnf::correlation

The raw correlation value of the received ack frame

§ rssi

int8_t _apimac_mcpsdatacnf::rssi

The RF power of the received ack frame in units dBm

§ frameCntr

uint32_t _apimac_mcpsdatacnf::frameCntr

Frame counter value used (if any) for the transmitted frame


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale