TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_mlmeassociatecnf Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_assocStatus_t status
 
uint16_t assocShortAddress
 
ApiMac_sec_t sec
 

Detailed Description

MAC_MLME_ASSOCIATE_CNF type

Field Documentation

§ status

ApiMac_assocStatus_t _apimac_mlmeassociatecnf::status

Status of associate attempt

§ assocShortAddress

uint16_t _apimac_mlmeassociatecnf::assocShortAddress

If successful, the short address allocated to this device

§ sec

ApiMac_sec_t _apimac_mlmeassociatecnf::sec

The security parameters for this message


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale