TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_mlmeassociatersp Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_sec_t sec
 
ApiMac_sAddrExt_t deviceAddress
 
uint16_t assocShortAddress
 
ApiMac_assocStatus_t status
 

Detailed Description

MLME associate response type

Field Documentation

§ sec

ApiMac_sec_t _apimac_mlmeassociatersp::sec

The security parameters for this message

§ deviceAddress

ApiMac_sAddrExt_t _apimac_mlmeassociatersp::deviceAddress

The address of the device requesting association

§ assocShortAddress

uint16_t _apimac_mlmeassociatersp::assocShortAddress

The short address allocated to the device

§ status

ApiMac_assocStatus_t _apimac_mlmeassociatersp::status

The status of the association attempt


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale