TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_mlmepollcnf Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_status_t status
 
uint8_t framePending
 

Detailed Description

MAC_MLME_POLL_CNF type

Field Documentation

§ status

ApiMac_status_t _apimac_mlmepollcnf::status

status of the poll request

§ framePending

uint8_t _apimac_mlmepollcnf::framePending

Set if framePending bit in data packet is set


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale