TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_mlmestartreq Struct Reference

#include <api_mac.h>

Data Fields

uint32_t startTime
 
uint16_t panId
 
uint8_t logicalChannel
 
uint8_t channelPage
 
uint8_t phyID
 
uint8_t beaconOrder
 
uint8_t superframeOrder
 
bool panCoordinator
 
bool batteryLifeExt
 
bool coordRealignment
 
ApiMac_sec_t realignSec
 
ApiMac_sec_t beaconSec
 
ApiMac_mpmParams_t mpmParams
 
bool startFH
 

Detailed Description

MLME start request type

Field Documentation

§ startTime

uint32_t _apimac_mlmestartreq::startTime

The time to begin transmitting beacons relative to the received beacon

§ panId

uint16_t _apimac_mlmestartreq::panId

The PAN ID to use. This parameter is ignored if panCoordinator is FALSE

§ logicalChannel

uint8_t _apimac_mlmestartreq::logicalChannel

The logical channel to use. This parameter is ignored if panCoordinator is FALSE

§ channelPage

uint8_t _apimac_mlmestartreq::channelPage

The channel page to use. This parameter is ignored if panCoordinator is FALSE

§ phyID

uint8_t _apimac_mlmestartreq::phyID

PHY ID corresponding to the PHY descriptor to use

§ beaconOrder

uint8_t _apimac_mlmestartreq::beaconOrder

The exponent used to calculate the beacon interval

§ superframeOrder

uint8_t _apimac_mlmestartreq::superframeOrder

The exponent used to calculate the superframe duration

§ panCoordinator

bool _apimac_mlmestartreq::panCoordinator

Set to TRUE to start a network as PAN coordinator

§ batteryLifeExt

bool _apimac_mlmestartreq::batteryLifeExt

If this value is TRUE, the receiver is disabled after MAC_BATT_LIFE_EXT_PERIODS full backoff periods following the interframe spacing period of the beacon frame

§ coordRealignment

bool _apimac_mlmestartreq::coordRealignment

Set to TRUE to transmit a coordinator realignment prior to changing the superframe configuration

§ realignSec

ApiMac_sec_t _apimac_mlmestartreq::realignSec

Security parameters for the coordinator realignment frame

§ beaconSec

ApiMac_sec_t _apimac_mlmestartreq::beaconSec

Security parameters for the beacon frame

§ mpmParams

ApiMac_mpmParams_t _apimac_mlmestartreq::mpmParams

MPM (multi-PHY layer management) parameters

§ startFH

bool _apimac_mlmestartreq::startFH

Indicates whether frequency hopping needs to be enabled


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale