TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_mlmesyncreq Struct Reference

#include <api_mac.h>

Data Fields

uint8_t logicalChannel
 
uint8_t channelPage
 
uint8_t phyID
 
uint8_t trackBeacon
 

Detailed Description

MAC_MlmeSyncReq type

Field Documentation

§ logicalChannel

uint8_t _apimac_mlmesyncreq::logicalChannel

The logical channel to use

§ channelPage

uint8_t _apimac_mlmesyncreq::channelPage

The channel page to use

§ phyID

uint8_t _apimac_mlmesyncreq::phyID

PHY ID corresponding to the PHY descriptor to use

§ trackBeacon

uint8_t _apimac_mlmesyncreq::trackBeacon

Set to TRUE to continue tracking beacons after synchronizing with the first beacon. Set to FALSE to only synchronize with the first beacon


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale