TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_sec Struct Reference

#include <api_mac.h>

Data Fields

uint8_t keySource [APIMAC_KEY_SOURCE_MAX_LEN]
 
uint8_t securityLevel
 
uint8_t keyIdMode
 
uint8_t keyIndex
 

Detailed Description

Common security type

Field Documentation

§ keySource

uint8_t _apimac_sec::keySource[APIMAC_KEY_SOURCE_MAX_LEN]

Key source

§ securityLevel

uint8_t _apimac_sec::securityLevel

Security Level

§ keyIdMode

uint8_t _apimac_sec::keyIdMode

Key identifier mode

§ keyIndex

uint8_t _apimac_sec::keyIndex

Key index


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale