TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_secdevicedescriptor Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_deviceDescriptor_t devInfo
 
ApiMac_frameCntr_tframeCntr
 
bool exempt
 

Detailed Description

Security Device Descriptor

Field Documentation

§ devInfo

ApiMac_deviceDescriptor_t _apimac_secdevicedescriptor::devInfo

Device information

§ frameCntr

ApiMac_frameCntr_t* _apimac_secdevicedescriptor::frameCntr

The incoming frame counter of the device. This value is used to ensure sequential freshness of frames. API_MAX_NODE_KEY_ENTRIES needs to match the value in macCfg.

§ exempt

bool _apimac_secdevicedescriptor::exempt

Device may override the minimum security level settings.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale