TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_securitykeyentry Struct Reference

#include <api_mac.h>

Data Fields

uint8_t keyEntry [APIMAC_KEY_MAX_LEN]
 
uint8_t keyIndex
 
uint32_t frameCounter
 

Detailed Description

MAC key entry structure

Field Documentation

§ keyEntry

uint8_t _apimac_securitykeyentry::keyEntry[APIMAC_KEY_MAX_LEN]

The 128-bit key

§ keyIndex

uint8_t _apimac_securitykeyentry::keyIndex

the key's index - unique

§ frameCounter

uint32_t _apimac_securitykeyentry::frameCounter

The key's frame counter


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale