TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_securitypibdeviceentry Struct Reference

#include <api_mac.h>

Data Fields

uint16_t deviceIndex
 
ApiMac_securityDeviceDescriptor_t deviceEntry
 

Detailed Description

Security PIB device entry for a Get/Set ApiMac_securityAttribute_deviceEntry

Field Documentation

§ deviceIndex

uint16_t _apimac_securitypibdeviceentry::deviceIndex

index into the macDeviceTable

§ deviceEntry

ApiMac_securityDeviceDescriptor_t _apimac_securitypibdeviceentry::deviceEntry

Place to put the requested data


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale