TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_securitypiblevelentry Struct Reference

#include <api_mac.h>

Data Fields

uint8_t levelIndex
 
ApiMac_securityLevelDescriptor_t levelEntry
 

Detailed Description

Security PIB level entry for a Get/Set ApiMac_securityAttribute_securityLevelEntry

Field Documentation

§ levelIndex

uint8_t _apimac_securitypiblevelentry::levelIndex

index into the macSecurityLevelTable

§ levelEntry

ApiMac_securityLevelDescriptor_t _apimac_securitypiblevelentry::levelEntry

Place to put the requested data


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale