TI-15.4 Stack API  4.20.00.14
Data Fields
ApiMac_sAddr_t Struct Reference

#include <api_mac.h>

Data Fields

union {
   uint16_t   shortAddr
 
   ApiMac_sAddrExt_t   extAddr
 
addr
 
ApiMac_addrType_t addrMode
 

Detailed Description

MAC address type field structure

Field Documentation

§ shortAddr

uint16_t ApiMac_sAddr_t::shortAddr

16 bit address

§ extAddr

ApiMac_sAddrExt_t ApiMac_sAddr_t::extAddr

Extended address

§ addr

union { ... } ApiMac_sAddr_t::addr

The address can be either a long address or a short address depending the addrMode field.

§ addrMode

ApiMac_addrType_t ApiMac_sAddr_t::addrMode

Address type/mode


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale