TI BLE5-Stack API Documentation
2.02.03.00
|
Handle Value Indication format. More...
Data Fields | |
uint16 | handle |
Handle of the attribute that has been changed (must be first field) | |
uint16 | len |
Length of value. | |
uint8 * | pValue |
Current value of the attribute (0 to ATT_MTU_SIZE-3) | |
Handle Value Indication format.
for method ATT_HANDLE_VALUE_IND